This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

some errors with my custom usecase based MCFW in DM8148 evm

Hi,

    when I run my usecase vcam_display in dvr_rdk4.0 on the TI DM8148 evm, It always failed , I alse use the camera/IF of the dm8148 with adding ISS iss_03_50_00_00, the following is some information about  my enviroment:

# Invoking configuro...
making package.mak (because of package.bld) ...
Memory Map - 1024MB DDR, 384MB Linux
  0x80000000     +-------------------+
         ^       |                   |
         |       |  256 MB           | Linux
         |       |                   |
         |       +-------------------+
         |       |  158MB             | (SR1) Bitstream buffer
         |       |                   | Cached on A8. Cached on M3, although access by DMAs
         |       +-------------------+
         +       |   6 MB          | Video M3 Code
       512 MB    +-------------------+
         |       |   2 MB         | Video  M3 Data
         |       +-------------------+
         |       |   4 MB            | VPSS  M3 Code
         |       +-------------------+
         |       |   4 MB           | VPSS  M3 Data
         |       +-------------------+
         |       |   4096 KB         | DSP Code
         |       +-------------------+
         v       |   26 MB           | DSP Data
  0xA0000000     +-------------------+
         ^       |   256 MB           | Tiled 8-bit + 16-bit region
         |       +-------------------+
         |       |  224 MB           | (SR2) Frame Buffer Region - <VPSS - Video M3 Frame Buf>
         |       +-------------------+  
         +       |                   |
       512 MB    |  17.5 MB          | (SR0) Syslink MsgQ/IPC List MP - <Non-cached on M3>
         +       +-------------------+
         |       |  256 KB           | Video M3 exception context
         |       +-------------------+  
         |       |  256KB            | Vpss M3 exception context
         |       +-------------------+  
         |       |  4 MB             | VPSS M3 - VPDMA Descriptor
         |       +-------------------+
         |       |  4 MB             | VPSS M3 - FBDev Shared Memory
         |       +-------------------+
         |       |  4 MB             | Host - VPSS M3 Notify(For FBDev)
         |       +-------------------+
         v       |  2 MB             | Remote Debug Print
   0xC0000000    +-------------------+
 ###
 ### Total DDR usage in MB = 1024 MB ###
 ###

but  there are some errors when I run my usecae VCam+vdis in DM8148,let me see the following :


/opt/dvr_rdk/ti814x
root@dm814x:/opt/dvr_rdk/ti814x# ./load.sh
Attached to slave procId 2.
Loaded file ../firmware/dvr_rdk_fw_m3vpss_1024M_256M.xem3 on slave procId 2.
Started slave procId 2.
After Ipc_loadcallback status [0x00000000]
 [m3vpss ]      ISS Freq  : 400 MHz
After Ipc_startcallback status [0x00000000]
 [m3vpss ] ***** VPSS Firmware build time 18:06:55 Mar 22 2014  EDG gcc 3.0 mode
 [m3vpss ] ***** SYSTEM  : Frequency <ORG> - 200000000, <NEW> - 200000000
 [m3vpss ] notify_attach  rtnVal  0
 [m3vpss ] initProxyServer  rtnVal  0
 [m3vpss ] 
 [m3vpss ]  *** UTILS: CPU KHz = 400000 Khz ***
 [m3vpss ] 
 [m3vpss ]  51: SYSTEM  : System Common Init in progress !!!
 [m3vpss ]  51: SYSTEM: IPC init in progress !!!
 [m3vpss ]  51: SYSTEM: Attaching to [HOST] ...
 [m3vpss ]  54: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
Attached to slave procId 1.
Loaded file ../firmware/dvr_rdk_fw_m3video_1024M_256M.xem3 on slave procId 1.
Started slave procId 1.
After Ipc_loadcallback status [0x00000000]
After Ipc_startcallback status [0x00000000]
 [m3video]      ISS Freq  : 400 MHz
 [m3video] ***** VIDEO Firmware build time 18:08:01 Mar 22 2014  EDG gcc 3.0 mode
 [m3video] ***** SYSTEM  : Frequency <ORG> - 200000000, <NEW> - 200000000
 [m3video] 
 [m3video]  *** UTILS: CPU KHz = 400000 Khz ***
 [m3video] 
 [m3video]  235: SYSTEM  : System Common Init in progress !!!
 [m3video]  235: SYSTEM: IPC init in progress !!!
 [m3video]  235: SYSTEM: Attaching to [HOST] ...
 [m3video]  239: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
Attached to slave procId 0.
Loaded file ../firmware/dvr_rdk_fw_c6xdsp_1024M_256M.xe674 on slave procId 0.
Started slave procId 0.
After Ipc_loadcallback status [0x00000000]
After Ipc_startcallback status [0x00000000]
 [c6xdsp ]      DSP Freq  : 500 MHz
 [m3video]  384: SYSTEM: Attaching to [DSP] ... SUCCESS !!!
 [m3video]  388: SYSTEM: Attaching to [VPSS-M3] ... SUCCESS !!!
 [m3vpss ]  386: SYSTEM: Attaching to [DSP] ... SUCCESS !!!
 [c6xdsp ] ***** VIDEO Firmware build time 18:05:03 Mar 22 2014  EDG gcc 3.0 mode
 [m3video]  388: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_1] ...
 [m3vpss ]  388: SYSTEM: Attaching to [VIDEO-M3] ... SUCCESS !!!
 [c6xdsp ] ***** SYSTEM  : Frequency <ORG> - 500000000, <NEW> - 500000000
 [m3video]  389: SYSTEM: Creating MsgQ [VIDEO-M3_MSGQ] ...
 [m3vpss ]  388: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_2] ...
 [c6xdsp ] 
 [m3video]  389: SYSTEM: Creating MsgQ [VIDEO-M3_ACK_MSGQ] ...
 [m3vpss ]  389: SYSTEM: Creating MsgQ [VPDMA: Module install successful, device major num = 251
DRV: Module install successful

 [c6xdsp ]  ***DRV: Module built on Mar 22 2014 15:40:58
 UTILS: CPU KHz = 500000 Khz ***
 [m3video]  391: SYSTEM: Notify register to [HOST] line 0, event 15 ...
 [m3vpss ]  389: SYSTEM: Creating MsgQ [VPSS-M3_ACK_MSGQ] ...
 [c6xdsp ] 
 [m3video]  392: SYSTEM: Notify register to [DSP] line 0, event 15 ...
 [m3vpss ]  391: SYSTEM: Notify register to [HOST] line 0, event 15 ...
 [c6xdsp ]  1: SYSTEM  : System Common Init in progress !!!
 [m3video]  392: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ...
 [m3vpss ]  391: SYSTEM: Notify register to [DSP] line 0, event 15 ...
 [c6xdsp ]  1: SYSTEM: IPC init in progress !!!
 [m3video]  392: SYSTEM: IPC init DONE !!!
 [m3vpss ]  392: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ...
 [c6xdsp ]  1: SYSTEM: Attaching to [HOST] ...
 [m3vpss ]  392: SYSTEM: IPC init DONE !!!
 [c6xdsp ]  4: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
 [c6xdsp ]  6: SYSTEM: Attaching to [VIDEO-M3] ... SUCCESS !!!
 [c6xdsp ]  8: SYSTEM: Attaching to [VPSS-M3] ... SUCCESS !!!
 [c6xdsp ]  8: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_0] ...
 [c6xdsp ]  8: SYSTEM: Creating MsgQ [DSP_MSGQ] ...
 [c6xdsp ]  8: SYSTEM: Creating MsgQ [DSP_ACK_MSGQ] ...
 [c6xdsp ]  9: SYSTEM: Notify register to [HOST] line 0, event 15 ...
 [c6xdsp ]  9: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ...
 [c6xdsp ]  9: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ...
 [c6xdsp ]  9: SYSTEM: IPC init DONE !!!
 [c6xdsp ]  12: MEM: Shared Region 2: Base = 0xb0000000, Length = 0x0e000000 (224 MB)
 [c6xdsp ]  12: MEM: ERROR: SharedRegion_setEntry (2, 0x9efeef5c) FAILED !!!  (status=-1)
 [m3video]  401: MEM: Shared Region 2: Base = 0xb0000000, Length = 0x0e000000 (224 MB)
 [m3vpss ]  401: MEM: Shared Region 2: Base = 0xb0000000, Length = 0x0e000000 (224 MB)
 [m3video]  401: MEM: Shared Region 1: Base = 0x90000000, Length = 0x09e00000 (158 MB)
 [m3vpss ]  401: MEM: Shared Region 1: Base = 0x90000000, Length = 0x09e00000 (158 MB)
 [m3video]  404: SYSTEM  : System Common Init Done !!!
 [m3vpss ]  403: SYSTEM  : System Common Init Done !!!
 [m3video]  404: SYSTEM  : System Video Init in progress !!!
 [m3vpss ]  403: SYSTEM  : System VPSS Init in progress !!!
 [m3video]  404: SYSTEM  : System Video Init Done !!!
 [m3vpss ]  404: SYSTEM: All VPDMA Free !!!
 [m3video]  405: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_0] in region 0 ...
 [m3video]  405: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_0] in region 0 ...
 [m3video]  405: SYSTEM: ListElem Shared Addr = 0xbe173e00
 [m3video]  408: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_1] in region 0 ...
 [m3video]  409: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_1] in region 0 ...
 [m3video]  409: SYSTEM: ListElem Shared Addr = 0xbe177300
 [m3video]  417: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_19] in region 0 ...
 [m3video]  418: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_19] in region 0 ...
 [m3video]  418: SYSTEM: ListElem Shared Addr = 0xbe17a800
 [m3video]  421: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_20] in region 0 ...
 [m3vpss ] === I2C0/2 Clk is active ===
 [m3video]  421: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_20] in region 0 ...
 [m3vpss ] PLATFORM: UNKNOWN CPU detected, defaulting to VPS_PLATFORM_CPU_REV_2_1
 [m3video]  422: SYSTEM: ListElem Shared Addr = 0xbe1a0000
 [m3vpss ]  PLATFORM: UNKNOWN CPU detected, defaulting to ISS_PLATFORM_CPU_REV_2_1
 [m3video]  425: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_21] in region 0 ...
 [m3vpss ]  428: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_0] in region 0 ...
 [m3video]  425: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_21] in region 0 ...
 [m3vpss ]  428: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_0] in region 0 ...
 [m3video]  426: SYSTEM: ListElem Shared Addr = 0xbe1c5800
 [m3vpss ]  429: SYSTEM: ListElem Shared Addr = 0xbe1eb000
 [m3vpss ]  432: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_1] in region 0 ...
 [m3video]  445: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_24] in region 0 ...
 [m3vpss ]  432: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_1] in region 0 ...
 [m3video]  446: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_24] in region 0 ...
 [m3vpss ]  432: SYSTEM: ListElem Shared Addr = 0xbe1ee500
 [m3video]  446: SYSTEM: ListElem Shared Addr = 0xbe1f1a00
 [m3vpss ]  453: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_19] in region 0 ...
 [m3video]  449: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_25] in region 0 ...
 [m3vpss ]  453: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_19] in region 0 ...
 [m3video]  450: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_25] in region 0 ...
 [m3vpss ]  454: SYSTEM: ListElem Shared Addr = 0xbe22d000
 [m3video]  450: SYSTEM: ListElem Shared Addr = 0xbe20f500
 [m3vpss ]  457: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_20] in region 0 ...
 [m3video]  452: HDVICP: Doing PRCM for IVAHD[0] ...
 [m3vpss ]  457: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_20] in region 0 ...
 [m3video]  452: HDVICP: PRCM for IVAHD[0] ... DONE.
 [m3vpss ]  458: SYSTEM: ListElem Shared Addr = 0xbe252800
 [m3video]  454: UTILS: DMA: HWI Create for INT62 !!!
 [m3vpss ]  461: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_21] in region 0 ...
 [m3video]  455: SYSTEM  : ISS Init in progress !!!
 [m3vpss ]  462: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_21] in region 0 ...
 [m3video]  455: SYSTEM  : ISS Power-ON in progress !!!
 [m3vpss ]  462: SYSTEM: ListElem Shared Addr = 0xbe278000
 [m3video]  465: SYSTEM  : ISS Power-ON in progress DONE !!!
 [m3vpss ]  464: SYSTEM : HDVPSS Drivers Version: HDVPSS_01_00_01_37
 [m3video]  465: SYSTEM  : ISS Init in progress DONE !!!
 [m3vpss ]  464: SYSTEM  : FVID2 Init in progress !!!
 [m3video]  465: VCOP BOOST BIT is Set
 [m3video]  466: SYSTEM  : Initializing Links !!!
 [c6xdsp ] Remote Debug Shared Memory @ 0xbfe00000
 [m3video] Remote Debug Shared Memory @ 0xbfe10820
 [m3vpss ] Remote Debug Shared Memory @ 0xbfe21040
 [m3video]  466: SYSTEM  : FREE SPACE : System Heap      = 6279248 B, Mbx = 10240 msgs)
 [m3vpss ] TILER_STATS: CNT :8BIT
 [m3video]  466: SYSTEM  : FREE SPACE : SR0 Heap         = 15609344 B (14 MB)
 [m3vpss ] TILER_STATS: CNT RESOLUTION:    16384 x 8192
 [m3video]  466: SYSTEM  : FREE SPACE : Frame Buffer     = 234880896 B (223 MB)
 [m3vpss ] TILER_STATS: BUCKET RESOLUTION: 16384 x 8188
 [m3video]  466: SYSTEM  : FREE SPACE : Bitstream Buffer = 165674880 B (157 MB)
 [m3vpss ] TILER_STATS: NUM FREE BUCKETS:  1
 [m3video]  466: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
 [m3video]  469: SYSTEM  : FREE SPACE : Tiler 8-bit      = 134152192 B (127 MB)  - TILER ON
 [m3vpss ] TILER_STATS: NUM USED BUCKETS:  0
 [m3video]  469: SYSTEM  : FREE SPACE : Tiler 16-bit     = 134217728 B (128 MB)  - TILER ON
 [m3vpss ] TILER_STATS: TOTAL FREE AREA:   134152192 (99 %)
 [m3video]  538: SYSTEM  : Initializing Links ... DONE !!!
 [m3vpss ] TILER_STATS: TOTAL USED AREA:   0 (0 %)
 [m3vpss ] TILER_STATS: CNT :16BIT
 [m3vpss ] TILER_STATS: CNT RESOLUTION:    32768 x 4096
 [m3vpss ] TILER_STATS: BUCKET RESOLUTION: 32768 x 4096
 [m3vpss ] TILER_STATS: NUM FREE BUCKETS:  1
 [m3vpss ] TILER_STATS: NUM USED BUCKETS:  0
 [m3vpss ] TILER_STATS: TOTAL FREE AREA:   134217728 (100 %)
 [m3vpss ] TILER_STATS: TOTAL USED AREA:   0 (0 %)
 [m3vpss ] PLATFORM: UNKNOWN CPU detected, defaulting to VPS_PLATFORM_CPU_REV_2_1
 [m3vpss ]  552: SYSTEM  : FVID2 Init in progress DONE !!!
 [m3vpss ]  552: SYSTEM  : ISS Init in progress !!!
 [m3vpss ]  552: SYSTEM  : ISS Power-ON in progress !!!
 [m3vpss ]  562: SYSTEM  : ISS Power-ON in progress DONE !!!
 [m3vpss ]  562: SYSTEM  : ISS Init in progress DONE !!!
 [m3vpss ]  562: VCOP BOOST BIT is Set
 [m3vpss ]  562: SYSTEM  : Device Init in progress !!!
 [m3vpss ]  I2C0: Passed for address 0x18 !!!
 [c6xdsp ]  1012: MEM: Shared Region 1: Base = 0x90000000, Length = 0x09e00000 (158 MB)
 [c6xdsp ]  1013: SYSTEM  : System Common Init Done !!!
 [c6xdsp ]  1011: SYSTEM  : System DSP Init in progress !!!
 [c6xdsp ]  1012: SYSTEM  : RpeServer_init() done... Ret Val 0!!!
 [c6xdsp ]  1017: SYSTEM: Creating ListMP [DSP_IPC_OUT_19] in region 0 ...
 [c6xdsp ]  1017: SYSTEM: Creating ListMP [DSP_IPC_IN_19] in region 0 ...
 [c6xdsp ]  1018: SYSTEM: ListElem Shared Addr = 0xbe29d800
 [c6xdsp ]  1019: SYSTEM: Creating ListMP [DSP_IPC_OUT_20] in region 0 ...
 [c6xdsp ]  1019: SYSTEM: Creating ListMP [DSP_IPC_IN_20] in region 0 ...
 [c6xdsp ]  1019: SYSTEM: ListElem Shared Addr = 0xbe2c3000
 [c6xdsp ]  1020: SYSTEM: Creating ListMP [DSP_IPC_OUT_21] in region 0 ...
 [c6xdsp ]  1020: SYSTEM: Creating ListMP [DSP_IPC_IN_21] in region 0 ...
 [c6xdsp ]  1020: SYSTEM: ListElem Shared Addr = 0xbe2e8800
 [c6xdsp ]  1021: SYSTEM: Creating ListMP [DSP_IPC_OUT_24] in region 0 ...
 [c6xdsp ]  1022: SYSTEM: Creating ListMP [DSP_IPC_IN_24] in region 0 ...
 [c6xdsp ]  1022: SYSTEM: ListElem Shared Addr = 0xbe30e000
 [c6xdsp ]  1023: SYSTEM: Creating ListMP [DSP_IPC_OUT_25] in region 0 ...
 [c6xdsp ]  1023: SYSTEM: Creating ListMP [DSP_IPC_IN_25] in region 0 ...
 [c6xdsp ]  1023: SYSTEM: ListElem Shared Addr = 0xbe32bb00
 [c6xdsp ] !!WARNING.Resource already registered:2
 [c6xdsp ]  1022: SYSTEM  : Initializing Links !!!
 [c6xdsp ]  1024: SYSTEM  : FREE SPACE : System Heap      = 6393472 B, Mbx = 10240 msgs)
 [c6xdsp ]  1040: SYSTEM  : Initializing Links ... DONE !!!
 [c6xdsp ]  1040: SYSTEM  : System DSP Init Done !!!
 [m3vpss ]  I2C0: Passed for address 0x2d !!!
 [m3vpss ]  I2C0: Passed for address 0x30 !!!
 [m3vpss ]  I2C0: Passed for address 0x34 !!!
 [m3vpss ]  I2C0: Passed for address 0x4b !!!
 [m3vpss ]  I2C0: Passed for address 0x66 !!!
 [m3vpss ]  3163: SYSTEM  : Device Init in progress DONE !!!
 [m3vpss ]      HDVPSS Freq  : 220 MHz
 [m3vpss ]  3218: SYSTEM  : System VPSS Init Done !!!
 [m3vpss ]  3219: UTILS: DMA: HWI Create for INT63 !!!
 [m3vpss ]  3220: SYSTEM  : Initializing Links !!!
 [m3vpss ]  3220: SYSTEM  : FREE SPACE : System Heap      = 248944 B, Mbx = 10240 msgs)
 [m3vpss ]  3220: SYSTEM  : FREE SPACE : SR0 Heap         = 14905344 B (14 MB)
 [m3vpss ]  3220: SYSTEM  : FREE SPACE : Frame Buffer     = 230570880 B (219 MB)
 [m3vpss ]  3221: SYSTEM  : FREE SPACE : Bitstream Buffer = 165674880 B (157 MB)
 [m3vpss ] TILER_STATS: CNT :8BIT
 [m3vpss ] TILER_STATS: CNT RESOLUTION:    16384 x 8192
 [m3vpss ] TILER_STATS: BUCKET RESOLUTION: 16384 x 8188
 [m3vpss ] TILER_STATS: NUM FREE BUCKETS:  1
 [m3vpss ] TILER_STATS: NUM USED BUCKETS:  0
 [m3vpss ] TILER_STATS: TOTAL FREE AREA:   134152192 (99 %)
 [m3vpss ] Received character 's'
 [m3vpss ] TILER_STATS: TOTAL USED AREA:   0 (0 %)
 [c6xdsp ] Remote Debug Shared Memory @ 0xbfe00000
 [m3video] Remote Debug Shared Memory @ 0xbfe10820
 [m3vpss ] Remote Debug Shared Memory @ 0xbfe21040
 [m3video] Received character 's'
 [c6xdsp ] Remote Debug Shared Memory @ 0xbfe00000
 [m3video] Remote Debug Shared Memory @ 0xbfe10820
 [m3vpss ] Remote Debug Shared Memory @ 0xbfe21040
 [c6xdsp ] Received character 's'
/opt/dvr_rdk/ti814x
 [m3vpss ] TILER_STATS: CNT :16BIT
 [m3vpss ] TILER_STATS: CNT RESOLUTION:    32768 x 4096
[module] vpss probe done.
 [m3vpss ] TILER_STATS: BUCKET RESOLUTION: 32768 x 4096
 [m3vpss ] TILER_STATS: NUM FREE BUCKETS:  1
[module] ti81xxfb probe done.
 [m3vpss ] TILER_STATS: NUM USED BUCKETS:  0
 [m3vpss ] TILER_STATS: TOTAL FREE AREA:   134217728 (100 %)
HDMI W1 rev 4.0
HDMI CEC Spec version 1.2
 [m3vpss ] TILER_STATS: TOTAL USED AREA:   0 (0 %)
 [m3vpss ]  3222: SYSTEM  : FREE SPACE : Tiler 8-bit      = 134152192 B (127 MB)  - TILER ON
 [m3vpss ]  3223: SYSTEM  : FREE SPACE : Tiler 16-bit     = 134217728 B (128 MB)  - TILER ON
 [m3vpss ]  3398: SYSTEM  : Initializing Links ... DONE !!!
 [m3vpss ]  3398: SYSTEM  : Set Static L3 pressure for HDVPSS as High
I2C No Ack

HDMI failed to read E-EDID
 
 ORG 0x46c00524: 0
 NEW 0x46c00524: 2
 
root@dm814x:/opt/dvr_rdk/ti814x# ./run.sh

 =========
 Main Menu
 =========

 1: 4CH VCAP + VENC + VDEC + VDIS  - Progressive SD Encode + Decode
 2: 8CH <D1+CIF> VCAP + VENC + VDEC + VDIS  - Progressive SD Encode + Decode
 3: 16CH RT VCAP + VENC + VDEC + VDIS  - Progressive SD Encode + Decode
 4: 16CH NRT <D1+CIF> VCAP + VENC + VDEC + VDIS  - Progressive SD Encode + Decode
 5:               VDEC + VDIS  - SD/HD Decode ONLY
 8: Vcap + Vdisp (sii9135 test)
 9: Vcam + Vdisp (vc0356 test)
 a: Vcap + Venc + Vdisp (sii9135 test)
 b: Vcam + Venc + Vdisp (vc0356 test)


 e: Exit

 Enter Choice: 9
--------------- CHANNEL DETAILS-------------
Disp Channels => 16
-------------------------------------------
 0: SYSTEM: System Common Init in progress !!!
 0: SYSTEM: IPC init in progress !!!
 17: SYSTEM: CPU [DSP] syslink proc ID is [0] !!!
 17: SYSTEM: CPU [VIDEO-M3] syslink proc ID is [1] !!!
 17: SYSTEM: CPU [VPSS-M3] syslink proc ID is [2] !!!
 17: SYSTEM: CPU [HOST] syslink proc ID is [3] !!!
 17: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_3] ...
 20: SYSTEM: Creating MsgQ [HOST_MSGQ] ...
 22: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ...
 23: SYSTEM: Opening MsgQ [DSP_MSGQ] ...
 24: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...
 24: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
 25: SYSTEM: Notify register to [DSP] line 0, event 15 ...
 26: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ...
 27: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ...
 27: SYSTEM: IPC init DONE !!!
 28: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ...
 30: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ...
 32: SYSTEM: ListElem Shared Addr = 0x40717880
 33: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ...
 35: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ...
 36: SYSTEM: ListElem Shared Addr = 0x4074ca80
 38: SYSTEM: Creating ListMP [HOST_IPC_OUT_19] in region 0 ...
 40: SYSTEM: Creating ListMP [HOST_IPC_IN_19] in region 0 ...
 41: SYSTEM: ListElem Shared Addr = 0x40781c80
 42: SYSTEM: Creating ListMP [HOST_IPC_OUT_20] in region 0 ...
 44: SYSTEM: Creating ListMP [HOST_IPC_IN_20] in region 0 ...
 46: SYSTEM: ListElem Shared Addr = 0x407c4f80
 47: SYSTEM: Creating ListMP [HOST_IPC_OUT_21] in region 0 ...
 49: SYSTEM: Creating ListMP [HOST_IPC_IN_21] in region 0 ...
 50: SYSTEM: ListElem Shared Addr = 0x40808280
 72: SYSTEM: System Common Init Done !!!
 [host] HDMI Ctrl :Initializing
 [host] HDMI Ctrl :Initialized
 [FBDEV]
 [FBDEV] FB: Starting !!!
 [FBDEV] FB: Opened device [/dev/fb0] (fd=21) !!!
 [FBDEV]
 [FBDEV] Fix Screen Info
 [FBDEV] ---------------
 [FBDEV] Line Length - 1600
 [FBDEV] Physical Address = 87e00000
 [FBDEV] Buffer Length = 2097152
 [FBDEV]
 [FBDEV]
 [FBDEV] Var Screen Info
 [FBDEV] ---------------
 [FBDEV] Xres - 800
 [FBDEV] Yres - 600
 [FBDEV] Xres Virtual - 800
 [FBDEV] Yres Virtual - 600
 [FBDEV] Bits Per Pixel - 16
 [FBDEV] Pixel Clk - 6734
 [FBDEV] Rotation - 0
 [FBDEV]
 [FBDEV]
 [FBDEV] Reg Params Info
 [FBDEV] ---------------
 [FBDEV] region 0, postion 0 x 0, prioirty 1
 [FBDEV] first 1, last 1
 [FBDEV] sc en 0, sten en 0
 [FBDEV] tran en 0, type 0, key 0
 [FBDEV] blend 0, alpha 0
 [FBDEV] bb en 0, alpha 0
 [FBDEV]
 [FBDEV]
 [FBDEV] ### BUF SIZE = 960000 Bytes !!!
 [FBDEV]
 [FBDEV] FB: Opened device [/dev/fb2] (fd2=22) !!!
 [FBDEV]
 [FBDEV] Fix Screen Info
 [FBDEV] ---------------
 [FBDEV] Line Length - 1440
 [FBDEV] Physical Address = 88000000
 [FBDEV] Buffer Length = 1048576
 [FBDEV]
 [FBDEV]
 [FBDEV] Var Screen Info
 [FBDEV] ---------------
 [FBDEV] Xres - 720
 [FBDEV] Yres - 480
 [FBDEV] Xres Virtual - 720
 [FBDEV] Yres Virtual - 480
 [FBDEV] Bits Per Pixel - 16
 [FBDEV] Pixel Clk - 18518
 [FBDEV] Rotation - 0
 [FBDEV]
 [FBDEV]
 [FBDEV] Reg Params Info
 [FBDEV] ---------------
 [FBDEV] region 0, postion 0 x 0, prioirty 1
 [FBDEV] first 1, last 1
 [FBDEV] sc en 0, sten en 0
 [FBDEV] tran en 0, type 0, key 0
 [FBDEV] blend 0, alpha 0
 [FBDEV] bb en 0, alpha 0
 [FBDEV]
 [FBDEV]
 [FBDEV] ### BUF SIZE = 691200 Bytes !!!
 [FBDEV]
 [FBDEV]
 [FBDEV] Fix Screen Info
 [FBDEV] ---------------
 [FBDEV] Line Length - 1600
 [FBDEV] Physical Address = 87e00000
 [FBDEV] Buffer Length = 2097152
 [FBDEV]
 [FBDEV]
 [FBDEV] Var Screen Info
 [FBDEV] ---------------
 [FBDEV] Xres - 800
 [FBDEV] Yres - 600
 [FBDEV] Xres Virtual - 800
 [FBDEV] Yres Virtual - 600
 [FBDEV] Bits Per Pixel - 16
 [FBDEV] Pixel Clk - 6734
 [FBDEV] Rotation - 0
 [FBDEV]
 [FBDEV]
 [FBDEV] Reg Params Info
 [FBDEV] ---------------
 [FBDEV] region 0, postion 0 x 0, prioirty 1
 [FBDEV] first 1, last 1
 [FBDEV] sc en 0, sten en 0
 [FBDEV] tran en 0, type 0, key 0
 [FBDEV] blend 0, alpha 0
 [FBDEV] bb en 0, alpha 0
 [FBDEV]
 [FBDEV]
 [FBDEV] ### BUF SIZE = 960000 Bytes !!!
 [FBDEV]
 [FBDEV]
 [FBDEV] Fix Screen Info
 [FBDEV] ---------------
 [FBDEV] Line Length - 1440
 [FBDEV] Physical Address = 88000000
 [FBDEV] Buffer Length = 1048576
 [FBDEV]
 [FBDEV]
 [FBDEV] Var Screen Info
 [FBDEV] ---------------
 [FBDEV] Xres - 720
 [FBDEV] Yres - 480
 [FBDEV] Xres Virtual - 720
 [FBDEV] Yres Virtual - 480
 [FBDEV] Bits Per Pixel - 16
 [FBDEV] Pixel Clk - 18518
 [FBDEV] Rotation - 0
 [FBDEV]
 [FBDEV]
 [FBDEV] Reg Params Info
 [FBDEV] ---------------
 [FBDEV] region 0, postion 0 x 0, prioirty 1
 [FBDEV] first 1, last 1
 [FBDEV] sc en 0, sten en 0
 [FBDEV] tran en 0, type 0, key 0
 [FBDEV] blend 0, alpha 0
 [FBDEV] bb en 0, alpha 0
 [FBDEV]
 [FBDEV]
 [FBDEV] ### BUF SIZE = 691200 Bytes !!!
 [FBDEV]
 [FBDEV] grpx_fb_draw ...
 [FBDEV] grpx_fb_draw ... Done !!!
 [FBDEV] grpx_fb_draw ...
 [FBDEV] grpx_fb_draw ... Done !!!
 [FBDEV] FB: Start DONE !!!
 [FBDEV]
 288: MCFW  : CPU Revision [ES2.1] !!!
MultiCh_detectBoard()  exit !MultiCh_detectBoard()
SYSTEM_LINK_ID_CAMERA begin
 System_ipcMsgQSendMsg starting
 [m3vpss ]  38350: CAMERA: Create in progress !!!
 [m3vpss ] FVID2_create  starting!!!!
 [m3vpss ]  38350: CAMERA: Create in progress !!!
 [m3vpss ] Create global VP camera handle  ing
 [m3vpss ]  38400: Assertion @ Line: 495 in links_m3vpss/camera/cameraLink_drv.c: pObj->fvidHandleVipAll != NULL : failed !!!
[m3vpss ]  38350: CAMERA: Create in progress !!!
 [m3vpss ] FVID2_create  starting!!!!
 [m3vpss ]  38350: CAMERA: Create in progress !!!
 [m3vpss ] Create global VP camera handle  ing
 [m3vpss ]  38400: Assertion @ Line: 495 in links_m3vpss/camera/cameraLink_drv.c: pObj->fvidHandleVipAll != NULL : failed !!!


I have taken several days on it ,hower , I still can't solve it ,please give  me some advices about  it

thanks in advance

regards,

shawn

  • Hi Shawn,

     

    DVR-RDK does not support capture from Camera, you will have to IPNC RDK to use camera link and iss software. Also as far as i know 8148 EVM does not support sensor based capture, You will require IPNC hardware to capture from sensor.

     

    Regards,

    Brijesh

  • hi Brijesh,

        But I see the datasheet of DM8148 and found that  there are a module about ISS,let's see the following:

    Imaging Subsystem(ISS)
    ProcessorCore
    – CameraSensorConnection
    • NEON™MultimediaArchitecture
    • ParallelConnectionforRaw(up to 16-Bit)
    • SupportsInteger andFloatingPoint
    andBT.656/BT.1120(8-/16-bit)
    • Jazelle®RCTExecutionEnvironment
    – Image SensorInterface (ISIF)forHandling
    • ARM®Cortex™-A8MemoryArchitecture
    Image/Video DataFromtheCameraSensor
    – 32K-ByteInstruction andDataCaches
    – Resizer
    – 512K-ByteL2Cache
    • ResizingImage/Video From1/16xto 8x
    – 64K-ByteRAM, 48K-ByteBootROM
    • GeneratingTwoDifferentResizing
    • TMS320C674x™Floating-PointVLIWDSP
    OutputsConcurrently


    so I think that ISS software also can be used in 8148, because of 8148 is pin-to-pin with dm8127~

     Regards,

    Shawn

  • Hi Shawn,

     

    This is the list of features supported by the TI8148 chip, but this also should be supported by the EVM or software that you are using. EVM does not support any sensor based capture, nor does DVR-RDK. DVR-RDK supports VIP based capture, For sensor/ISS capture, you will have to use IPNC-RDK.

     

    Regards,

    Brijesh

  • hi Regards,

     thanks for your kindly answer!