This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

connect error

I use C5509A and SEEDXDS 510-USB2.0 Emulator,but when connecting,the error as follow:

Error connecting to the target: Error 0x80002240/-121 Fatal Error during: Initialization, OCS, Control, This error was generated by TI's USCIF driver.

SC_ERR_CMD_HANDLE <-121> A bad controller handle has been given to a function, either before attempting to open the controller, or after having opened the controller and ignored its error status. Valid controller handles are generated when attempts to open the controller return a clean error status.

Sequence ID: 0 Error Code: -121 Error Class: 0x80002240 I/O Port = 240

Board Name: C5509A  SEEDXDS510USB  Emulator Cpu Name: TMS320C5500_0

Abort:  Close Code Composer Studio. Retry:  Try to connect to the target again. Cancel:  Remain disconnected from the target Diagnostic: Run diagnostic utility.

need help !

Thank you very much!

zhf