This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

enc framerate

now my link structure  like following:

if i do just 1 loopback test ,the enc FPS of channel 0 is about 53-54(enc parameter set is 60FPS) OR the enc FPS of channel 0 is about 25(enc parameter set is 30FPS)

but when i do the 2 loopback test,the FPS of channel 0 is about 31-35(enc parameter set is 60FPS) OR the enc FPS of channel 0 is about 16-18(enc parameter set is 30FPS)

the following is the log:

3566.encFps.log