Other Parts Discussed in Thread: TMS320C6678
Hi,
Recently, I was reading the evmc6678l.gel file which found in MCSDK packet. Here, I have some questions about the xmc_setup() function shows bellow:
According to the C66xx CoerPacs User Guide, firstly, shouldn't it be 4KB in the note line /*……(64KB)*/ since the last 5 bit of XMPAX2_H forms B (01011) ? then ,why the last 8 bit are 11111111(FF) in XMPAX2_L, you kown there contains 2 reserved bit that is bit 7 & bit6, it's recommended 0 in the C66xx CoerPacs User Guide.
Still, if the seg size is 4KB, I want to know why it's 4KB instead of 8KB,16KB,etc. Then I checked the memory map in TMS320C6678's datasheet to find out the address that meet the xmc_setup() showed above. It's follows:
Here ,I was confused since the length is just 512B ,but it's defined 4KB in xmc_setup() ,won't it cause memory over flow? Once ,I thought maybe we can use the reserved space followed the 512B DDR3 EMIF configuration space , now I don't think its right . Could you help resolve my confusion? Thanks.
Best Regards,
Philly.