The board is myselve's , which use C6678, the envirment is CCS5.3
when I use noboot mode, I can connect simulator and load program without problems, but when I write a program into flash(just a simple helloworld program and I use writting tools in MCSDK), then choose SPI mode, a problem named 1143 occured when I connect the simulator.
Now I have verified that the data in the flash is correct and, I can go through smoothly with another board which has nearly same design.
How should I do with it? Every suggestion is appreciative.