This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cap out format set

hi all ,my cap parameter set is 

pCaptureInstPrm->inDataFormat           = SYSTEM_DF_YUV422P;

 

so if i set the 

pCaptureOutPrm->dataFormat              = SYSTEM_DF_YUV422P;

 

then it will have the error:

[m3vpss ] 65996: CAPTURE: Create in progress !!!
[m3vpss ] 66026: CAPTURE: VIP0 PortA capture mode is [16-bit, Non-mux Discrete Sync - ACTVID_VSYNC] !!!
[m3vpss ] 66026: Assertion @ Line: 832 in links_m3vpss/capture/captureLink_drv.c: pInst->captureVipHandle != NULL : failed !!!

so why?

tks