Hello,
I'd like to use UART1(ttyO0) with CTS, but uart1_tx send data while uart1_cts is de-asserted (level high). I also checked UART2(ttyO1) and UART3(ttyO2) with each CTS on J16 header pin of EVM3517 application board. These didnt send during de-asserted. I mean the behavior of UART1 is not correct. I processed software with PSPv04.02.00.07 (Linux SDK v6) and BSL from Logic PD. Please give me advices.
Best Regards,