This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65910 with AM3352

Other Parts Discussed in Thread: TPS65910, AM3352, TPS65910A

Hello,

We'd like to ask about TPS65910.

<Question1>
On the document 「am335x_evm_15X15 baseboard.dsn」, why doesn't the VDD3(SW3) connect to Vbus of AM3352? 
So, the source VDD3(SW3) is DC-DC voltage, does't it fit for USB power?

<Question2> 
On the document 「TPS65910Ax User's Guide for AM335X processor」,
pull up resistanse of SCL and SDA is 1.2kΩ.

When we use only Fast mode or slave mode, how much value of resistance should we use?
In case of only using Fast mode (400 Kbps) : XXkΩ
In case of only using slave mode(100 Kbps) : XXkΩ

<Question3>
We could not find out the content of rush current of the TPS65910A.
If the value of the rush current is higher than the value of over rated current,  what will the device behave?

Kind regards,

Hirotaka Matsumoto