Other Parts Discussed in Thread: ADS1258, TMS320C5515
The EVM/MDK boots fine without the ECG AFE, but once the AFE is attached, the LED D1 (XF signal) stays on and the board does not boot from the SPI eeprom. I think there is a conflict on the SPI bus, since the AFE A/D and the EVM SPI EEPROM are using the same SPI port. Has anyone also seen this problem?
Thanks,
Bin