This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSK6713 audio codec issue

Hello,

Im doing a project on realtime feedforward adaptive noise cancellation using DSK6713, and I need to access 2 audio inputs simultaneously. But i found they are multiplexed, so is there a way that I can use this DSK to solve the problem?

Thank You

Rakshith

  • Rakshith,

    The audio input connections on the DSK6713 are stereo so you could have two mono audio input on each side of the stereo input connector.

    Will this solve your problem? If not, then you can get an audio add-on card that will plug onto the daughtercard connectors of the DSK. Search the web for "DSK6713 audio daughtercard" (no quotes) or other similar keywords.

    Regards,
    RandyP

  • Hi Rakshith,

    Thanks for your post.

    Even in my opinion, you cannot access 2 independant audio inputs except the possibility of 2 mono inputs as Randy suggested.

    Regards,

    Sivaraj K

    -------------------------------------------------------------------------------------------------------
    Please click the Verify Answer button on this post if it answers your question.
    -------------------------------------------------------------------------------------------------------