This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

built AM335x Image can't boot from SD card

I built an image using the: ti-sdk-am335x-evm-06.00.00.00

and it booted successfully after being flashed to the SD card. A colleague of mine made a different image and can boot it via TFTP, but when I tried to use the same image and boot via SD card method it won't work and constantly spits back messages about "read only filesystem"

mdev: can't create 'usbdev1.1': Read-only file system
mdev: can't create 'mice': Read-only file system
mdev: can't create 'event0': Read-only file system
mdev: can't create 'event1': Read-only file system
mdev: can't create 'mouse0': Read-only file system

The full log is attached:

CCCCCCCC
U-Boot SPL 2013.01.01 (Mar 18 2014 - 14:29:14)
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO 
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0 
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO 
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0 
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img


U-Boot 2013.01.01 (Mar 18 2014 - 14:29:14)

I2C:   ready
DRAM:  512 MiB
WARNING: Caches not enabled
NAND:  256 MiB
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - bad CRC, using default environment

musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO 
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0 
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO 
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0 
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net:   <ethaddr> not set. Validating first E-fuse MAC
cpsw, usb_ether
Hit any key to stop autoboot:  1  0 
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
** Unable to read file uEnv.txt **
reading uImage
3152224 bytes read in 348 ms (8.6 MiB/s)
Booting from mmc ...
## Booting kernel from Legacy Image at 80007fc0 ...
   Image Name:   Linux-3.2.03.2-am335xpsp
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3152160 Bytes = 3 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   XIP Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[    0.000000] Linux version 3.2.03.2-am335xpsp (mike@mike-VirtualBox) (gcc vers
ion 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313
 - Linaro GCC 2013.03) ) #1 Tue Mar 18 13:39:44 EDT 2014
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instructio
n cache
[    0.000000] Machine: am335xevm
[    0.000000] Memory policy: ECC disabled, Data cache writeback
[    0.000000] AM335X ES1.0 (sgx neon )
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pag
es: 130048
[    0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 r
o rootfstype=ext3 rootwait ip=none
[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Memory: 512MB = 512MB total
[    0.000000] Memory: 513260k/513260k available, 11028k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
[    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)
[    0.000000]       .text : 0xc0008000 - 0xc0586000   (5624 kB)
[    0.000000]       .init : 0xc0586000 - 0xc05be000   ( 224 kB)
[    0.000000]       .data : 0xc05be000 - 0xc0627b60   ( 423 kB)
[    0.000000]        .bss : 0xc0627b84 - 0xc0656724   ( 187 kB)
[    0.000000] NR_IRQS:396
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrup
ts
[    0.000000] Total of 128 interrupts on 1 active controller
[    0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[    0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 13
1071999ms
[    0.000000] Console: colour dummy device 80x30
[    0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[    0.058959] pid_max: default: 32768 minimum: 301
[    0.059082] Security Framework initialized
[    0.059173] Mount-cache hash table entries: 512
[    0.059570] CPU: Testing write buffer coherency: ok
[    0.080078] omap_hwmod: pruss: failed to hardreset
[    0.081237] print_constraints: dummy: 
[    0.081634] NET: Registered protocol family 16
[    0.083862] OMAP GPIO hardware version 0.1
[    0.086486] omap_mux_init: Add partition: #1: core, flags: 0
[    0.088500]  omap_i2c.1: alias fck already exists
[    0.089477]  omap2_mcspi.1: alias fck already exists
[    0.089691]  omap2_mcspi.2: alias fck already exists
[    0.090667]  edma.0: alias fck already exists
[    0.090667]  edma.0: alias fck already exists
[    0.090698]  edma.0: alias fck already exists
[    0.117919] bio: create slab <bio-0> at 0
[    0.120239] SCSI subsystem initialized
[    0.121887] usbcore: registered new interface driver usbfs
[    0.122192] usbcore: registered new interface driver hub
[    0.122406] usbcore: registered new device driver usb
[    0.122558] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[    0.122863] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[    0.123992] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[    0.125915] tps65910 1-002d: JTAGREVNUM 0x0
[    0.128326] print_constraints: VRTC: 
[    0.129760] print_constraints: VIO: at 1800 mV 
[    0.132080] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal 
[    0.134399] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal 
[    0.135375] print_constraints: VDD3: 5000 mV 
[    0.136810] print_constraints: VDIG1: at 1800 mV 
[    0.138214] print_constraints: VDIG2: at 1800 mV 
[    0.139648] print_constraints: VPLL: at 1800 mV 
[    0.141082] print_constraints: VDAC: at 1800 mV 
[    0.142486] print_constraints: VAUX1: at 1800 mV 
[    0.143951] print_constraints: VAUX2: at 3300 mV 
[    0.145385] print_constraints: VAUX33: at 3300 mV 
[    0.146789] print_constraints: VMMC: at 3300 mV 
[    0.147308] tps65910 1-002d: No interrupt support, no core IRQ
[    0.148712] Advanced Linux Sound Architecture Driver Version 1.0.24.
[    0.149902] Switching to clocksource gp timer
[    0.165679] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[    0.165863] musb-hdrc musb-hdrc.0: dma type: pio
[    0.166198] MUSB0 controller's USBSS revision = 4ea20800
[    0.166839] musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using 
PIO, IRQ 18
[    0.166992] musb-hdrc musb-hdrc.1: dma type: pio
[    0.167297] MUSB1 controller's USBSS revision = 4ea20800
[    0.167480] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[    0.167572] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus numbe
r 1
[    0.167694] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    0.167694] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=
1
[    0.167724] usb usb1: Product: MUSB HDRC host driver
[    0.167724] usb usb1: Manufacturer: Linux 3.2.03.2-am335xpsp musb-hcd
[    0.167755] usb usb1: SerialNumber: musb-hdrc.1
[    0.168548] hub 1-0:1.0: USB hub found
[    0.168579] hub 1-0:1.0: 1 port detected
[    0.169158] musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 using
 PIO, IRQ 19
[    0.169586] NET: Registered protocol family 2
[    0.169769] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[    0.170196] TCP established hash table entries: 16384 (order: 5, 131072 bytes
)
[    0.170471] TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
[    0.170654] TCP: Hash tables configured (established 16384 bind 16384)
[    0.170654] TCP reno registered
[    0.170684] UDP hash table entries: 256 (order: 0, 4096 bytes)
[    0.170715] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[    0.170898] NET: Registered protocol family 1
[    0.171173] RPC: Registered named UNIX socket transport module.
[    0.171203] RPC: Registered udp transport module.
[    0.171203] RPC: Registered tcp transport module.
[    0.171203] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.192626] VFS: Disk quotas dquot_6.5.2
[    0.192687] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.193267] msgmni has been set to 1002
[    0.196472] alg: No test for stdrng (krng)
[    0.197174] io scheduler noop registered
[    0.197174] io scheduler deadline registered
[    0.197265] io scheduler cfq registered (default)
[    0.201019] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[    0.819244] console [ttyO0] enabled
[    0.823516] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[    0.831390] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[    0.839141] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[    0.846954] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[    0.854736] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[    0.863037] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00
[    0.879394] brd: module loaded
[    0.887512] loop: module loaded
[    0.891021] i2c-core: driver [tsl2550] using legacy suspend method
[    0.897460] i2c-core: driver [tsl2550] using legacy resume method
[    0.903900] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    0.917816] Detected a daughter card on AM335x EVM..
[    0.922851] CPLD version: CPLD1.0F
[    0.926696] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    0.941864] Board name: A33515BB
[    0.945251] Board version: 1.4A
[    0.948516] SKU: SKU#01
[    0.951599] The board is general purpose EVM in profile 0
[    0.958282]  da8xx_lcdc.0: alias fck already exists
[    0.963836] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel
[    0.987945] Console: switching to colour frame buffer device 100x30
[    1.005035] omap-gpmc omap-gpmc: GPMC revision 6.0
[    1.010040] Registering NAND on CS0
[    1.014495]  omap_i2c.2: alias fck already exists
[    1.019805] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 100 kHz
[    1.026306] tsl2550 2-0039: standard operating mode
[    1.032104] tsl2550 2-0039: support ver. 1.2 enabled
[    1.037933]  davinci-mcasp.1: alias fck already exists
[    1.043975]  omap_hsmmc.0: alias fck already exists
[    1.049407]  omap_hsmmc.2: alias fck already exists
[    1.054870] Configure Bluetooth Enable pin...
[    1.060913] registered am33xx_sr device
[    1.065155] _regulator_get: 2-0018 supply Vdd not found, using dummy regulato
r
[    1.072814] _regulator_get: 2-0018 supply Vdd_IO not found, using dummy regul
ator
[    1.101226] lis3lv02d: 8 bits 3DLH sensor found
[    1.190948] input: ST LIS3LV02DL Accelerometer as /devices/platform/lis3lv02d
/input/input0
[    1.202789] mtdoops: mtd device (mtddev=name/number) must be supplied
[    1.210083] omap2-nand driver initializing
[    1.214721] ONFI flash detected
[    1.218109] ONFI param page 0 valid
[    1.221801] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron MT29F2G
08ABAEAWP)
[    1.230377] Creating 8 MTD partitions on "omap2-nand.0":
[    1.235961] 0x000000000000-0x000000020000 : "SPL"
[    1.242340] 0x000000020000-0x000000040000 : "SPL.backup1"
[    1.249237] 0x000000040000-0x000000060000 : "SPL.backup2"
[    1.256164] 0x000000060000-0x000000080000 : "SPL.backup3"
[    1.263092] 0x000000080000-0x000000260000 : "U-Boot"
[    1.270263] 0x000000260000-0x000000280000 : "U-Boot Env"
[    1.277160] 0x000000280000-0x000000780000 : "Kernel"
[    1.285736] 0x000000780000-0x000010000000 : "File System"
[    1.395904] OneNAND driver initializing
[    1.401428] CAN device driver interface
[    1.405426] CAN bus driver for Bosch D_CAN controller 1.0
[    1.460540] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[    1.467010] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
[    1.474426] davinci_mdio.0: probed
[    1.477996] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
[    1.485717] usbcore: registered new interface driver zd1201
[    1.491760] usbcore: registered new interface driver cdc_ether
[    1.498016] usbcore: registered new interface driver cdc_eem
[    1.504089] usbcore: registered new interface driver dm9601
[    1.509948] cdc_ncm: 04-Aug-2011
[    1.513488] usbcore: registered new interface driver cdc_ncm
[    1.519409] Initializing USB Mass Storage driver...
[    1.524719] usbcore: registered new interface driver usb-storage
[    1.531005] USB Mass Storage support registered.
[    1.536285] mousedev: PS/2 mouse device common for all mice
[    1.543029] input: matrix-keypad as /devices/platform/matrix-keypad/input/inp
ut1
[    1.552093] input: ti-tsc as /devices/platform/omap/ti_tscadc/tsc/input/input
2
[    1.560729] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
[    1.567901] i2c /dev entries driver
[    1.572265] Linux video capture interface: v2.00
[    1.577423] usbcore: registered new interface driver uvcvideo
[    1.583435] USB Video Class driver (1.1.1)
[    1.588592] lm75 2-0048: hwmon0: sensor 'tmp275'
[    1.596405] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    1.605041] cpuidle: using governor ladder
[    1.609802] cpuidle: using governor menu
[    1.617797] omap4_aes_mod_init: loading AM33X AES driver
[    1.623504] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[    1.630065] omap4_aes_probe: probe() done
[    1.634735] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[    1.640899] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[    1.655731] omap4_sham_probe: probe() done
[    1.665832] usbcore: registered new interface driver usbhid
[    1.671691] usbhid: USB HID core driver
[    1.676391] tiadc tiadc: attached adc driver
[    1.681640] usbcore: registered new interface driver snd-usb-audio
[    1.690063] _regulator_get: 2-001b supply IOVDD not found, using dummy regula
tor
[    1.697937] _regulator_get: 2-001b supply DVDD not found, using dummy regulat
or
[    1.705627] _regulator_get: 2-001b supply AVDD not found, using dummy regulat
or
[    1.713317] _regulator_get: 2-001b supply DRVDD not found, using dummy regula
tor
[    1.723876] asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok
[    1.731689] ALSA device list:
[    1.734802]   #0: AM335X EVM
[    1.737792] oprofile: hardware counters not available
[    1.743103] oprofile: using timer interrupt.
[    1.747558] nf_conntrack version 0.5.0 (8019 buckets, 32076 max)
[    1.754455] ip_tables: (C) 2000-2006 Netfilter Core Team
[    1.760131] TCP cubic registered
[    1.763519] NET: Registered protocol family 17
[    1.768188] can: controller area network core (rev 20090105 abi 8)
[    1.774749] NET: Registered protocol family 29
[    1.779388] can: raw protocol (rev 20090105)
[    1.783843] can: broadcast manager protocol (rev 20090105 t)
[    1.789794] Registering the dns_resolver key type
[    1.794799] VFP support v0.3: implementor 41 architecture 3 part 30 variant c
 rev 3
[    1.802825] ThumbEE CPU extension supported.
[    1.807342] mux: Failed to setup hwmod io irq -22
[    1.812957] Power Management for AM33XX family
[    1.817840] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[    1.824554] Copied the M3 firmware to UMEM
[    1.828918] Cortex M3 Firmware Version = 0x18
[    1.833587] smartreflex smartreflex: am33xx_sr_probe: Zero NValue read from E
FUSE
[    1.841461] smartreflex: probe of smartreflex failed with error -22
[    1.848632] sr_init: platform driver register failed
[    1.858978] clock: disabling unused clocks to save power
[    1.878295] Detected MACID=0:18:31:8f:1b:7b
[    1.883819] cpsw: Detected MACID = 00:18:31:8f:1b:7c
[    1.889495] mmc0: new high speed SDHC card at address aaaa
[    1.896423] mmcblk0: mmc0:aaaa SU08G 7.40 GiB 
[    1.902862] input: gpio-keys as /devices/platform/gpio-keys/input/input3
[    1.910247]  mmcblk0: p1 p2
[    1.914337] omap_rtc am33xx-rtc: setting system clock to 2000-01-01 00:00:00 
UTC (946684800)
[    2.001281] kjournald starting.  Commit interval 5 seconds
[    2.007080] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[    2.014343] VFS: Mounted root (ext3 filesystem) readonly on device 179:2.
[    2.021850] Freeing init memory: 224K
[    2.045257] mmc1: card claims to support voltages below the defined range. Th
ese will be ignored.
[    2.066253] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
[    2.073364] mmc1: new SDIO card at address 0001
INIT: version 2.88 booting
mdev: can't create 'tty9': Read-only file system
mdev: can't create 'tty10': Read-only file system
mdev: can't create 'tty11': Read-only file system
mdev: can't create 'tty12': Read-only file system
mdev: can't create 'tty13': Read-only file system
mdev: can't create 'tty14': Read-only file system
mdev: can't create 'tty15': Read-only file system
mdev: can't create 'tty16': Read-only file system
mdev: can't create 'tty17': Read-only file system
mdev: can't create 'tty18': Read-only file system
mdev: can't create 'tty19': Read-only file system
mdev: can't create 'tty20': Read-only file system
mdev: can't create 'tty21': Read-only file system
mdev: can't create 'tty22': Read-only file system
mdev: can't create 'tty23': Read-only file system
mdev: can't create 'tty24': Read-only file system
mdev: can't create 'tty25': Read-only file system
mdev: can't create 'tty26': Read-only file system
mdev: can't create 'tty27': Read-only file system
mdev: can't create 'tty28': Read-only file system
mdev: can't create 'tty29': Read-only file system
mdev: can't create 'tty30': Read-only file system
mdev: can't create 'tty31': Read-only file system
mdev: can't create 'tty32': Read-only file system
mdev: can't create 'tty33': Read-only file system
mdev: can't create 'tty34': Read-only file system
mdev: can't create 'tty35': Read-only file system
mdev: can't create 'tty36': Read-only file system
mdev: can't create 'tty37': Read-only file system
mdev: can't create 'tty38': Read-only file system
mdev: can't create 'tty39': Read-only file system
mdev: can't create 'tty40': Read-only file system
mdev: can't create 'tty41': Read-only file system
mdev: can't create 'tty42': Read-only file system
mdev: can't create 'tty43': Read-only file system
mdev: can't create 'tty44': Read-only file system
mdev: can't create 'tty45': Read-only file system
mdev: can't create 'tty46': Read-only file system
mdev: can't create 'tty47': Read-only file system
mdev: can't create 'tty48': Read-only file system
mdev: can't create 'tty49': Read-only file system
mdev: can't create 'tty50': Read-only file system
mdev: can't create 'tty51': Read-only file system
mdev: can't create 'tty52': Read-only file system
mdev: can't create 'tty53': Read-only file system
mdev: can't create 'tty54': Read-only file system
mdev: can't create 'tty55': Read-only file system
mdev: can't create 'tty56': Read-only file system
mdev: can't create 'tty57': Read-only file system
mdev: can't create 'tty58': Read-only file system
mdev: can't create 'tty59': Read-only file system
mdev: can't create 'tty60': Read-only file system
mdev: can't create 'tty61': Read-only file system
mdev: can't create 'tty62': Read-only file system
mdev: can't create 'tty63': Read-only file system
mdev: can't create 'ptmx': Read-only file system
mdev: can't create 'ttyO0': Read-only file system
mdev: can't create 'ttyO1': Read-only file system
mdev: can't create 'ttyO2': Read-only file system
mdev: can't create 'ttyO3': Read-only file system
mdev: can't create 'ttyO4': Read-only file system
mdev: can't create 'ttyO5': Read-only file system
mdev: can't create 'ram4': Read-only file system
mdev: can't create 'ram5': Read-only file system
mdev: can't create 'ram6': Read-only file system
mdev: can't create 'ram7': Read-only file system
mdev: can't create 'ram8': Read-only file system
mdev: can't create 'ram9': Read-only file system
mdev: can't create 'ram10': Read-only file system
mdev: can't create 'ram11': Read-only file system
mdev: can't create 'ram12': Read-only file system
mdev: can't create 'ram13': Read-only file system
mdev: can't create 'ram14': Read-only file system
mdev: can't create 'ram15': Read-only file system
mdev: can't create 'loop0': Read-only file system
mdev: can't create 'loop1': Read-only file system
mdev: can't create 'loop2': Read-only file system
mdev: can't create 'loop3': Read-only file system
mdev: can't create 'loop4': Read-only file system
mdev: can't create 'loop5': Read-only file system
mdev: can't create 'loop6': Read-only file system
mdev: can't create 'loop7': Read-only file system
mdev: can't create 'mmcblk0': Read-only file system
mdev: can't create 'mmcblk0p1': Read-only file system
mdev: can't create 'mmcblk0p2': Read-only file system
mdev: can't create 'rfkill': Read-only file system
mdev: can't create 'crypto': Read-only file system
mdev: can't create 'hw_random': Read-only file system
mdev: can't create 'loop-control': Read-only file system
mdev: can't create 'ubi_ctrl': Read-only file system
mdev: can't create 'psaux': Read-only file system
mdev: can't create 'watchdog': Read-only file system
mdev: can't create 'cpu_dma_latency': Read-only file system
mdev: can't create 'network_latency': Read-only file system
mdev: can't create 'network_throughput': Read-only file system
mdev: can't create 'usbdev1.1': Read-only file system
mdev: can't create 'mice': Read-only file system
mdev: can't create 'event0': Read-only file system
mdev: can't create 'event1': Read-only file system
mdev: can't create 'mouse0': Read-only file system
mdev: can't create 'event2': Read-only file system
mdev: can't create 'event3': Read-only file system
mdev: can't create 'rtc0': Read-only file system
mdev: can't create 'timer': Read-only file system
mdev: can't create 'pcmC0D0p': Read-only file system
mdev: can't create 'pcmC0D0c': Read-only file system
mdev: can't create 'controlC0': Read-only file system
mdev: can't create 'full': Read-only file system
mdev: can't create 'vcs': Read-only file system
mdev: can't create 'vcsa': Read-only file system
mdev: can't create 'vcs1': Read-only file system
mdev: can't create 'vcsa1': Read-only file system
mdev: can't create 'mtd0ro': Read-only file system
mdev: can't create 'mtd1ro': Read-only file system
mdev: can't create 'mtd2ro': Read-only file system
mdev: can't create 'mtd3ro': Read-only file system
mdev: can't create 'mtd4ro': Read-only file system
mdev: can't create 'mtd5ro': Read-only file system
mdev: can't create 'mtd6ro': Read-only file system
mdev: can't create 'mtd7ro': Read-only file system
mdev: can't create 'i2c-1': Read-only file system
mdev: can't create 'i2c-2': Read-only file system
Starting Bootlog daemon: bootlogd: cannot find console device 252:0 under /dev
bootlogd.
Executing: /etc/rcS.d/S10init_ccf
mkdir: can't create directory '/var/tmp': Read-only file system
mount: mounting tmpfs on /var/tmp failed: No such file or directory
Configuring network interfaces... RTNETLINK answers: File exists
ifup: can't open '/var/run/ifstate': Read-only fINIT: Entering runlevel: 5
Starting syslog-ng:Error binding socket; addr='AF_UNIX(/dev/log)', error='Read-o
nly file system (30)'
Error initializing source driver; source='src_dev_log'
.
Executing: /etc/rc5.d/S20pcdd
Starting: pcd
Starting network management services: snmpd.
Starting internet superserver: xinetd.
Stopping Bootlog daemon: bootlogd.
snmpd[949]: Cannot find module (IP-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (IF-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (UDP-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (HOST-RESOURCES-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (SNMPv2-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (SNMPv2-SMI): At line 0 in (none)

snmpd[949]: Cannot find module (NOTIFICATION-LOG-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (UCD-SNMP-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (UCD-DEMO-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (SNMP-TARGET-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (NET-SNMP-AGENT-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (IPV6-ICMP-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (IPV6-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (IPV6-TCP-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (IPV6-UDP-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (SNMP-VIEW-BASED-ACM-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (SNMP-COMMUNITY-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (NET-SNMP-EXTEND-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (UCD-DLMOD-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (SNMP-FRAMEWORK-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (SNMP-MPD-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (SNMP-USER-BASED-SM-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (SNMP-NOTIFICATION-MIB): At line 0 in (none)

snmpd[949]: Cannot find module (SNMPv2-TM): At line 0 in (none)

snmpd[949]: Turning on AgentX master support.

snmpd[949]: Creating directory: /var/agentx

snmpd[949]: Failed to create the directory for the agentX socket: /var/agentx/ma
ster

snmpd[949]: Error: Couldn't open a master agentx socket to listen on (/var/agent
x/master): Unknown host (No such file or directory)

I'm trying to understand what in the build procedure (probably in the kernel not in the u-boot) would cause linux to act this way? My colleague and I are not sure what differences he made and I'm hoping that the log can be analyzed for some hints without having to dig through every little thing in the build procedure.

  • In the log:

    [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext3 rootwait ip=none

    Your rootfs is mounted as read-only. Please change your u-boot bootargs from 'ro' to 'rw'.

  • Thanks Bin Liu! That did allow the system to boot. One outstanding question however. When I compared the printenv from the working build, and this non-working build, I saw both were the same.

    I just checked again specifically looking at this line and indeed the "working" build that I created with the ti-sdk has the uboot variable set the same:

    mmcroot=/dev/mmcblk0p2 ro

    Why on the build that I made with the SDK can I boot with "ro" but when I try to boot with the build of my colleague I need to set it to "rw"?

     

  • Mike,

    Does your SD card which has the new uImage have the same rootfs package as that in the working SD card? Your log shows 'Executing: /etc/rcS.d/S10init_ccf', I am not sure where this script comes from, I don't see it on the SDK rootfs.

    If all the packages for partition 1 & 2 of the SD card come from the SDK, u-boot sets the rootfs mounted as ro as specified in 'mmcroot=' initially, then /etc/rcS.d/S10checkroot.sh remounts it to rw. I suspect your rootfs does not have checkroot.sh script, so further mounting failed.