This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 SPI-NOR FLASH boot problem



Dear TI engineers,

I'm booting my own board with C6678 from SPI Nor FLASH. In noboot mode, I can load and run my application with the simulator connected. But i cann't boot C6678 through SPI(from Nor FLASH).

The application is successfully writed into FLASH but the board is disconnected with the simulator immediately when I reset the board in SPI mode(error 1143 occured).

I have verified the code which has been writed into FLASH, it's corrected.

Could you please give me some advices?

Thank you!