This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with i2s write through DMA



IDE:CCS5.5

ChipSet:C5515 DSP

OS:WIN

Emulator:XDS100V1

Audio Settings: 16bit Little Endian,8000Sampling Rate

Problem:unable to listen playback through I2S via DMA

aic3204 settings:
   // Configure AIC3204

PAGE0

REG 1 =  1  // Reset codec
USBSTK5515_wait_Test( 200 ); // Wait

//Configure Power Supplies
PAGE 1 
REG 1 =  8  // Disable crude AVDD generation from DVDD
REG  2 =  1  // Enable Analog Blocks, use LDO power

// PLL and Clocks config and Power Up

PAGE 0

REG 27 =  0x0d  // I2S interface, 16 Bit, BCLK and WCLK is set as o/p ,DOUT High Impedence
REG 28 =  0x00  // Data ofset = 0
REG 4   =  3  // PLL setting: PLLCLK <- MCLK, CODEC_CLKIN <-PLL CLK
REG 6   =  4  // PLL setting: J = 4
REG  7  =  0x17  // PLL setting: HI_BYTE(D)
REG 8   =  0xc0  // PLL setting: LO_BYTE(D)
REG 30 =  0x88  // BCLK N Divider ->> DAC_CLK/N =(12288000/8) = 1.536MHz = 32*fs
REG 5   =  0xA4  // PLL setting: Power up PLL, P=2 and R=4
REG 13 =  0  // Hi_Byte(DOSR)
REG 14 =  0x80  // Lo_Byte(DOSR)
REG 20 =  0x80  // AOSR for AOSR = 128 ->> Use with PRB_R1 to PRB_R6, ADC Filter Type A)
REG 11 =  0x80+36  // Power up NDAC and set NDAC value to 36
REG 12 =  0x83  // Power up MDAC and set MDAC value to 3
REG 18 =  0x80+36  // Power up NADC and set NADC value to 36
REG 19 =  0x83  // Power up MADC and set MADC value to 3

// DAC ROUTING and Power Up

PAGE1

REG 12 = 0x08  // LDAC AFIR routed to HPL
REG 13 = 0x08 // RDAC AFIR routed to HPR
PAGE0

REG 64 = 0x02 // Left vol=right vol
REG 65 = 0x00 // Left DAC gain to 0dB VOL; Right tracks Left
REG 63 = 0xd4 // Power up left,right data paths and set channel
PAGE1

REG  16  = 6  // Unmute HPL , 6dB gain
REG  17 =  6  // Unmute HPR , 6dB gain
REG  9   = 0x30 // Power up HPL,HPR
I2S2 settings

short USBSTK5515_I2S_init(void)

{
	/* I2S settings */
	I2S2_SRGR = 0x0;
	I2S2_CR = 0x8010;    // 16-bit word, slave, enable I2C
	I2S2_ICMR = 0x3f ;    // Disable interrupts 0x3f for enable

	
	return 0;
}
dma settings:

PlayBuf = &g_DMA_PlayingBuf[0];

DMA1CH0TCR2 = 0x0204 ;// DMA_EN = 0, Destn Addr = Constant, Source Add Auto Inc, Sync Mode

src_add_P = (Uint32)PlayBuf  ;

if((src_add_P >= CSL_DMA_DARAM_START_ADDR) && (src_add_P <= CSL_DMA_DARAM_END_ADDR))
  src_add_P = (src_add_P << 1) + 0x010000 ;//BYTE ADDRESS TO DMA
else if((src_add_P >= CSL_DMA_SARAM_START_ADDR)&& (src_add_P <= CSL_DMA_SARAM_END_ADDR))
  src_add_P = (src_add_P << 1)+ 0x080000 ;// BYTE ADDRESS TO DMA

DMA1CH0SSAU = (Uint16) (src_add_P >> 16) ;

DMA1CH0SSAL = (Uint16) src_add_P ;

// Dest Address = I2S0 Address, No Inc

DMA1CH0DSAU = 0 ;

DMA1CH0DSAL = 0x2A0C ; //I2S2_W1_LSW_W Right Channel Tx Register Address of I2S2

//event sync..
// Select Event I2S2 to Trigger DMA in DMAnCESR
DMA1CESR1 = 0x0601 ;

DMA1CESR2 = 0x0000 ;

DMA1CH0TCR1 = DMA_PLAYBACK_BUFFER_SIZE * 4 ;	// Length = 240

DMA1CH0TCR2 = 0x0204 ;// DMA_EN = 0

despite of all proper settings also i am not able to acquire valid data from my HPR/HPL,when debugged while i was writing a particular data to the dma playback buffer i am not seeing the same data in the transmit register i.e, the dma is taking wrong data from its address,if you see the screen shot i have attached you can see the buffer content and the content at the tx register of that particular channel ,

when i have loaded the address it was properly loaded the 

byte  address  = 0x020000 << 1  + 0x080000 =>0xC0000 but 

,on every step in i am finding the DMA src address increment in unevenly why so ? should nt it be increment by 4 ? 

is that a debugger problem ?

what is the solution to my problem,am i using a wrong dma settings or what ? i really doubt on address the DMA is referring to !

PS:my playback dma buffer  is of size 50kB located in SARAM from x00040000 to x0004C800 

ScreenShots:

if any sample projects are available you can link them where i can follow up the settings