Hi,
I have to develop a secondary boot loader for DM6437 board. My plan is to create two section in NOR flash
1. App Boot loader (NOT ROM boot loader)
2. Application
On start-up, the ROM boot loader will load App boot loader, App boot loader will update the Application area if there is an update. Both App Boot loader and Application need to reside in NOR flash.
But on reading "Using the TMS320DM643x Bootloader" document , i cant find NOR flash boot option. There is only NAND flash boot option.
Can any one tell me ,this idea is feasible or not?
If it is feasible, can anyone provide me the documents or detailed information about NOR flash boot option in DM6437 board.
Regards,
Shihab