This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Crosscompiling from Win7 to Beaglebone Black with Qt

Hello,


I'm trying to compile a Qt 5.2 application from Win7 to Beaglebone Black. I found a tutorial with Qt 4.8

http://c2143.blogspot.de/2011/08/developping-for-qt-48-embedded-on.html

but it doesn´t work, the error meassage is:

generators/win32/msvc_vcproj.cpp:77:15: warning: anonymous type with no linkage used to declare variable '<anonymous struct> dotNetCombo []' with linkage [enabled by default]  } dotNetCombo[] = {
               ^
..\shared\profileevaluator.cpp: In member function 'ProFileEvaluator::Private::VisitReturn ProFileEvaluator::Private::evaluateConditionalFunction(const ProString&, const ProStringList&)':
..\shared\profileevaluator.cpp:2965:18: warning: variable 'ignore_error' set but not used [-Wunused-but-set-variable]
             bool ignore_error = false;
                  ^
Der Befehl "perl" ist entweder falsch geschrieben oder konnte nicht gefunden werden.
Der Befehl "perl" ist entweder falsch geschrieben oder konnte nicht gefunden werden.
process_begin: CreateProcess(NULL, arm-linux-gnueabi-g++ -c -pipe -g -Wall -W -D_REENTRANT -fPIC -DQT_SHARED -DQT_BUILD_CORE_LIB -DQT_NO_USING_NAMESPACE -DQT_NO_CAST_TO_ASCII -DQT_ASCII_CAST_WARNINGS -DQT_MOC_COMPAT -DQT_USE_QSTRINGBUILDER -DELF_INTERPRETER=\"\" -DQLIBRARYINFO_EPOCROOT -DHB_EXPORT=Q_CORE_EXPORT -D_LARGEFILE64_SOURCE -D_LARGEFILE_SOURCE -DQT_HAVE_MMX -DQT_HAVE_3DNOW -DQT_HAVE_SSE -DQT_HAVE_MMXEXT -DQT_HAVE_SSE2 -I../../mkspecs/linux-arm-gnueabi-g++ -I. -I../../include -I../../include/QtCore -Itmp/rcc/debug_shared -Iglobal -I../../tools/shared -I../3rdparty/harfbuzz/src -I../3rdparty/md5 -I../3rdparty/md4 -Itmp/moc/debug_shared -o tmp/obj/debug_shared/qatomic_arm.o arch/arm/qatomic_arm.cpp, ...) failed.
make (e=2): Das System kann die angegebene Datei nicht finden.
...

Have everybody an idee about this error, or better have everybody a Qt 5.2 (qmake) Version for Win7 to BBB.

Thank you for helping


Michael