This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRIO data transfer speed



Hi ,

I have configured my SRIO for 1 port 4x speed( 5 Gbps x4=20 Gbps.MYSNC =1 for port 0.path config=4,path mode=4

But I observe that profile time is as per 5 Gbps results,not 20 Gbps(I have referred .For example to transfer 4k bytes from dsp to end device,it takes 11 micro seconds if source address is L2 SRAM and 15 microS if its in DDR3.

What may be the reason for this.Please help ASAP

 

Thanks and Regards,

Thomas