Where can I go to get a better understanding of how the memory is partitioned between the two processors on the OMAP-L137
Of the 64 MBytes of SDRAM on the OMAP-L137 EVM board, how much can safely be used by the DSP without interfering with the ARM operation.
If I understand correctly, from looking at the Memory Map diagram in the EVM technical reference all 64 MBytes of SDRam is visible to the DSP. Does montevista use some of this 64 MByte space for its own purposes?
Thanks
Rich Bagdazian