Other Parts Discussed in Thread: TMS320DM8168
Hello,
We are using TMS320DM8168 interfaced with a NTSC/ PAL video decoder,whose output is driven w.r.t. falling clock edge.
TMS320DM8168 samples input data w.r.t. rising clock edge.
TMS320DM8168 datasheet page 264, mentions that at 165MHz, setup time required is 3.75nsec and hold time is 0nsec.
We are getting setup time violations on this interface and would like to know following:
1) At 108MHz input clock, will setup and hold timing requirement be the same?
2) If not, then provide for 108MHz the setup and hold timing requirement values.
3) Is it possible to change VINx port sampling from rising edge to falling edge?
Pls do revert on this at the earliest.
Thanks & Regards,
Roma Bhagat