This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

two capture makes Frame Rate reduce?



hi,all:

My env: dm8168 and dvr rdk 4.0

My chains: vcap->nsf->venc->vdec->sw->vdis.

      CAPTURE: when I only use VIP0 or VIPI , the encode FPS is ok.

      when I use two capture VIP0 and VIP1, the encode FPS reduce. For example, my capture: VIP0(1080P600) and VIP1(1080P10) .

       use  Vsys_printDetailedStatistics,we see the issue. (encode channel 0 FPS only 41 and encode channel1 FPS only 7).

       Anybody can help me? thanks!