I want to use some of the GPIO pins of the TMDSEVM6670L to establish a 10 Mbps link between two TMDSEVM6670Ls, is it possible? If it is, how should i do?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sy Huang,
GPIOs are not the right way to communicate between the two DSPs. There are many different peripherals available on the C6670, with several being available on the expansion connector, the AMC edge connector, or on other physical connectors, such as Ethernet.
Regards,
RandyP