This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352 power estimation

Other Parts Discussed in Thread: AM3352

Hi,

I am using the power estimation tool for estimating the power used by AM3352 and i got the following results -

  min max Leakage Active Average
VDD_MPU 1.13 1.13 0.099 0.511 0.609
VDD_CORE 0.91 0.91 0.067 0.222 0.289
VDDS_DPLL 1.80 1.80 0.000 0.009 0.009
VDDS_SRAM 1.80 1.80 0.008 0.000 0.008
VDDS_DDR 1.50 1.50 0.000 0.002 0.002
VDDS_1P8 1.80 1.80 0.000 0.008 0.008
VDDS_3P3 3.30 3.30 0.000 0.005 0.005
VDDA1P8V_USB0/1, VDDA_ADC 1.80 1.80 0.000 0.000 0.000
VDDA3P3V_USB0/1 3.30 3.30 0.000 0.000 0.000

I am assuming that the USB powers are zero because of some bug in the tool.

Other than this the VDDS_DDR current is just 2mA for for 60% EMIF utilization. Also 3.3V supply (VDDS_3P3) is used for multiple peripherals of AM3352 but the current is 5mA. Are these values fine?

Regards,

Nikhil