Other Parts Discussed in Thread: OMAPL138
Dear forum
I want realize a Poetable Video Recoder, a semplified version that only record the video in SD card ,and after read the SD
and send data via USB or SPI. No monitor or user interface.
I wold like compress data like MPEG 4 or H 264.
Device able to do this if find to be all the DaVinci family ,expecially DM64x ,DM38x ,DM35-6x,,all family whit fixed point processor or video coprocessor .
Because i would like to work whit a Floating Point because personal implementation of some algoritm , i woul like to work whit the OMAP L138 whit the C674x Floating point ,but nobody mention this device for compression.
Can you explain to me why ? A float processor is also a fix processor, so basically, OMAPL13x and DM6467 (ARM+ fix point) are not the same from a power calculation point ?
Thanks very much
Roberto