Hi
Till now I have been booting DM355 from NFS. Now I have transferred the contents to FLASH. I followed the steps given in A.5 (Getting started guide) and set bootargs as :
setenv bootargs 'mem=116M console=ttyS0,115200n8 root=/dev/mtdblock3 rw rootfstype=yaffs2 ip=10.20.21.15:10.20.21.12:10.20.1.1:255.255.0.0:::off'
This is the IP setting which had been working using NFS boot. The problem is that the FLASH boots correctly only when the serial port is connected to a computer. This is irrespective of which system I connect the serial port to. Can you please hep with the problem
Thanks