Hello,
Now, I'm checking the TMDXEVM3358 schematics.
Is any pull-up registers needed for GPMC pins; for example, GPMC_CSn0, GPMC_WPn and GPMC_WAIT0?
Because the internal pull-up registers are active, no pull-up registers are needed, I think.
Also, if the pull-up registers are connected, teach me recommended value.
And, if there are no recommended values, could you teach me the rise time for the GPMC input signal (NAND mode).
Best Regards.
Nomoto