This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DHCP client "Host name" advanced field



Hello I'm using NDK.

I enable dynamic IP (not v6), HTTP and DHCP CLIENT.

I write "tisoc" value in field "Host name".

This value is the name of the host in network ?

If I open Internet Explorer and I digit http://tisoc/home.htm no answer I obtain.

If I use IP address (I read from console  "Network Added: If-1:192.168.3.66") it works

http://192.168.3.66/home.htm

I don't understand how field "Host name" works.

Can someone help me ?

  • Hi Maro!

    Not (completly) sure since I never used BIOS on TI.

    But what you're trying to use is a feature from the DHCP server (running on your Router or anywhere in your LAN). This feature there enables the clients (your TI with DHCP client) to give a "hint" to the DHCP server for obtaining an IP address! This hint is also (sometimes) called "host"...


    This has nothing to do with DNS which you are trying to use in your browser in the address line....


    For this you need to look inside your Router (have a look for dnsmasq and others... :-)

    HTH. Salut, Joerg

  • And so, what is the meaning of field of "Host name" ?

  • As I said: I dont't use NDK and/or BIOS, but what I know about DHCP is that

    the term "hostname" in combination with a DHCP client hints to something like the following:

    http://www.cyberciti.biz/faq/howto-get-linux-static-dhcp-address/

    theoretical background would be:

    http://en.wikipedia.org/wiki/Dynamic_Host_Configuration_Protocol#DHCP_options

    and is table "Code 12"....

    This is excactly what I meant with "hinting the server" with our own "hostname"! :-)


    Kind regards, Joerg