Hi all:
I met a problem about DMVAL in appro 8127 RDK3.50.
DMVAL error:
[c6xdsp ] > DMVAL: Invalid timestamp in video frame!
sometimes it's:
[c6xdsp ] > DMVAL: DMVAL_IMG_YUV420_PLANARINTERLEAVED input image detected. Copying 92160 bytes of input into buffer#0 [c6xdsp ] DMVAL: [c6xdsp ] > DMVAL: Circular buffer pointer: Current = 0, Previous = 0, Oldest = 1. [c6xdsp ] > DMVAL: Exiting DMVAL_processInput. [c6xdsp ] DMVAL: [c6xdsp ] > DMVAL: Called DMVAL_resetMem for Bank#10199... [c6xdsp ] DMVAL: [c6xdsp ] > DMVAL: bytesRLE bytes exceeded. Out of memory!!! [c6xdsp ] DMVAL: [c6xdsp ] > DMVAL: Input invalid!
The difference of DMVAL parameters between original case and mine is the framerate. I gave 15fps and the original is 30fps.
I printed timestamps and can't find any reason to lead to the error.
Could anyone give me some help? Or supply some detailed docs about DMVAL?
Regards.
Lanston