Other Parts Discussed in Thread: AM3517
Hi All,
I am in the process of porting the linux kernel 3.14 version to AM3517 custom board.
I am using omap2plus_defconfig for building the kernel.
When the kernel loads it is hanging in the "Starting kernel ...". Even it is not doing the un compressing the images also. I have verified the Machine ID. The machine ID is correct. I enabled the early printk but i didnt get any logs
Please let me know if anything else i need to check.
Log:
4194304 bytes read: OK
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux-3.14.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3575880 Bytes = 3.4 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
announce_and_cleanup
Starting kernel ...
cleanup_before_linux
Thanks,
P.Ashok.