This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flashing MLO to NAND flash without CCS



Hello,

I need to flash MLO and u-boot.img to NAND flash (to address 0x0 and 0x80000), but that address space is externaly inaccessible. How can i do that with BDI3000? I have CCS but with free licence so BDI3000 is not supported. My board is custom made, based on AM335x EVM, without possibility of boot jumper configuring (NAND boot is the only option).

Thanks in advance,

Nemanja Golubovic