This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDR3 memory mapping

Hi!

I'm working with C6678 DSP. I'd like to use 4GB DDR3 at my custom board. As far I understand from C6678 datasheet each DSP core has max 2 GB memory area at 0x80000000 to access to external DDR3 memory. The 32-bit DSP logical address converts to 36-bit physical address by XMC. So my questions are:

1. Is max available to each DSP core DDR3 memory length 2 GB?

2. If I want to use 4 GB DDR3 I need to split it between DSP cores by configuring XMC MPAX segments for each core. Am I right?