Other Parts Discussed in Thread: OMAP3530
Hi,
We bought an OMAP3530 EVM with Mistral. There is some problems running the DSPLINK samples.
We are running on a NFS Server. Below is the error. I already read some topics about DSPLINK errors and checked memory maps, but I didnt made any changes in any file of DSPLINK and its samples. I'm just trying to use the samples to only after they are Ok, start to do my own code.
Any kind of help would be appreciated.
Thanks
root@omap3evm:/# ./messagegpp message.out 0
========== Sample Application : MESSAGE ==========
Entered MESSAGE_Create ()
Entered PROC_setup ()
linkCfg [0x0]
Entered DRV_Initialize ()
drvObj [0x37824]
arg [0x0]
Failure: Status:[0x80008008] File:[0x50c] Line:[370]
Leaving DRV_Initialize () status [0x80008008]
Failure: Status:[0x80008008] File:[0x200] Line:[238]
Leaving PROC_setup () status [0x80008008]
PROC_setup () failed. Status = [0x80008008]
Leaving MESSAGE_Create ()
Entered MESSAGE_Delete ()
Entered MSGQ_release ()
msgqQueue [0xffff]
Assertion failed (IS_VALID_MSGQ (msgqQueue)). File : msgq.c Line : 484
Failure: Status:[0x8000800b] File:[0x202] Line:[488]
Leaving MSGQ_release () status [0x8000800b]
MSGQ_release () failed. Status = [0x8000800b]
Entered MSGQ_transportClose ()
procId [0x0]
Failure: Status:[0x80008002] File:[0x202] Line:[227]
Leaving MSGQ_transportClose () status [0x80008002]
Entered PROC_stop ()
procId [0x0]
Failure: Status:[0x80008002] File:[0x200] Line:[1175]
Leaving PROC_stop () status [0x80008002]
Entered MSGQ_setErrorHandler ()
errorQueue [0xffff]
poolId [0xffff]
Entered DRV_Invoke ()
drvObj [0x0]
cmdId [0x6f0c]
arg1 [0xbe945c34]
arg2 [0x0]
Assertion failed (((drvObj != NULL) && (IS_OBJECT_VALID (drvObj, SIGN_DRV))) ||
((drvObj == NULL) && (cmdId == CMD_PROC_ATTACH))). File : drv_api.c Line : 509
Failure: Status:[0x80008002] File:[0x50c] Line:[1367]
Leaving DRV_Invoke () status [0x80008002]
Failure: Status:[0x80008002] File:[0x202] Line:[783]
Leaving MSGQ_setErrorHandler () status [0x80008002]
Entered MSGQ_close ()
msgqQueue [0xffff]
Assertion failed (IS_VALID_MSGQ (msgqQueue)). File : msgq.c Line : 335
Failure: Status:[0x8000800b] File:[0x202] Line:[339]
Leaving MSGQ_close () status [0x8000800b]
Entered POOL_close ()
poolId [0x0]
Failure: Status:[0x80008000] File:[0x203] Line:[228]
Leaving POOL_close () status [0x80008000]
Entered PROC_detach ()
procId [0x0]
Failure: Status:[0x80008000] File:[0x200] Line:[670]
Leaving PROC_detach () status [0x80008000]
Entered PROC_destroy ()
Failure: Status:[0x80008000] File:[0x200] Line:[351]
Failure: Status:[0x80008000] File:[0x200] Line:[435]
Leaving PROC_destroy () status [0x80008000]
Leaving MESSAGE_Delete ()
====================================================