Other Parts Discussed in Thread: AM3352
Hello Everyone,
I was previously using the ti-evm-sdk version 05.05 and I have switched to the version 06.00.00.00. I've completed the Uboot board port exercise and now can run uboot on my board (almost). The problem I'm facing is unclear to me and I was hoping to get some inputs / help.
I've enabled DEBUG option in Uboot and I'm attaching the log file from the serial console output. In the code I've also added several debug messages of my own - they all start with "*** SR:". The problem is with U-boot relocating - the execution seems to go off the rails in the function jump_to_image_no_args defined in spl.c. The last entry in the log file is debug("image entry point: 0x%X\n", spl_image->entry_point);
I am able to run my old U-boot on this board consistently (from sdk 05.05.00.00) but it seems that there are several changes made to the underlying u-boot code that I'm not able to trace the problem back. Any help is much appreciated - thank you.
Also I do have another question regarding some of the defines in the include/configs/am335x_evm.h file. What are these definitions for and how are they used?
#define CONFIG_SYS_LOAD_ADDR 0x81000000
#define CONFIG_SYS_TEXT_BASE 0x80800000
#define CONFIG_SYS_SPL_MALLOC_START 0x80208000
#define CONFIG_SYS_SPL_MALLOC_SIZE 0x00100000
Thank you for your replies and your patience.
Regards
Santhosh
=~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2014.04.02 17:19:35 =~=~=~=~=~=~=~=~=~=~=~= U-Boot SPL 2013.01.01 (Apr 02 2014 - 17:18:02) *** SR: DDR Frequency is 125 Mhz *** *** SR: Leaving s_init *** >>spl:board_init_r() *** SR: Entering am33xx_spl_board_init *** *** SR: DCDC1 - 1.8V *** *** SR: DCDC2 - 3.3V *** *** SR: DCDC3 - 1.1V *** *** SR: LDO1 - 1.8V *** *** SR: LDO2 - 3.3V *** *** SR: LDO3 - 1.8V *** *** SR: Leaving am33xx_spl_board_init *** boot device - 8 OMAP SD/MMC: 0 boot mode - FAT reading u-boot.img VFAT Support enabled FAT32, fat_sect: 32, fatlength: 1112 Rootdir begins at cluster: 2, sector: 2256, offset: 11a000 Data begins at: 2254 Sector size: 512, cluster size: 1 FAT read sect=2256, clust_size=1, DIRENTSPERBLOCK=16 RootMismatch: |mlo|| Rootvfatname: |u-boot.img| RootName: u-boot.img, start: 0x5390, size: 0x4267c Filesize: 271996 bytes 64 bytes gc - clustnum: 21392, startsect: 23646 Size: 271996, got: 64 spl: payload image: U-Boot 2013.01.01 for aa_hcc boa `: load addr: 0x807fffc0 size: 271996 reading u-boot.img VFAT Support enabled FAT32, fat_sect: 32, fatlength: 1112 Rootdir begins at cluster: 2, sector: 2256, offset: 11a000 Data begins at: 2254 Sector size: 512, cluster size: 1 FAT read sect=2256, clust_size=1, DIRENTSPERBLOCK=16 RootMismatch: |mlo|| Rootvfatname: |u-boot.img| RootName: u-boot.img, start: 0x5390, size: 0x4267c Filesize: 271996 bytes 271996 bytes FAT32: entry: 0x5390 = 21392, offset: 0x0290 = 656 FAT32: ret: 00005391, offset: 0290 FAT32: entry: 0x5391 = 21393, offset: 0x0291 = 657 FAT32: ret: 00005392, offset: 0291 FAT32: entry: 0x5392 = 21394, offset: 0x0292 = 658 FAT32: ret: 00005393, offset: 0292 FAT32: entry: 0x5393 = 21395, offset: 0x0293 = 659 FAT32: ret: 00005394, offset: 0293 FAT32: entry: 0x5394 = 21396, offset: 0x0294 = 660 FAT32: ret: 00005395, offset: 0294 FAT32: entry: 0x5395 = 21397, offset: 0x0295 = 661 FAT32: ret: 00005396, offset: 0295 FAT32: entry: 0x5396 = 21398, offset: 0x0296 = 662 FAT32: ret: 00005397, offset: 0296 FAT32: entry: 0x5397 = 21399, offset: 0x0297 = 663 FAT32: ret: 00005398, offset: 0297 FAT32: entry: 0x5398 = 21400, offset: 0x0298 = 664 FAT32: ret: 00005399, offset: 0298 FAT32: entry: 0x5399 = 21401, offset: 0x0299 = 665 FAT32: ret: 0000539a, offset: 0299 FAT32: entry: 0x539a = 21402, offset: 0x029a = 666 FAT32: ret: 0000539b, offset: 029a FAT32: entry: 0x539b = 21403, offset: 0x029b = 667 FAT32: ret: 0000539c, offset: 029b FAT32: entry: 0x539c = 21404, offset: 0x029c = 668 FAT32: ret: 0000539d, offset: 029c FAT32: entry: 0x539d = 21405, offset: 0x029d = 669 FAT32: ret: 0000539e, offset: 029d FAT32: entry: 0x539e = 21406, offset: 0x029e = 670 FAT32: ret: 0000539f, offset: 029e FAT32: entry: 0x539f = 21407, offset: 0x029f = 671 FAT32: ret: 000053a0, offset: 029f FAT32: entry: 0x53a0 = 21408, offset: 0x02a0 = 672 FAT32: ret: 000053a1, offset: 02a0 FAT32: entry: 0x53a1 = 21409, offset: 0x02a1 = 673 FAT32: ret: 000053a2, offset: 02a1 FAT32: entry: 0x53a2 = 21410, offset: 0x02a2 = 674 FAT32: ret: 000053a3, offset: 02a2 FAT32: entry: 0x53a3 = 21411, offset: 0x02a3 = 675 FAT32: ret: 000053a4, offset: 02a3 FAT32: entry: 0x53a4 = 21412, offset: 0x02a4 = 676 FAT32: ret: 000053a5, offset: 02a4 FAT32: entry: 0x53a5 = 21413, offset: 0x02a5 = 677 FAT32: ret: 000053a6, offset: 02a5 FAT32: entry: 0x53a6 = 21414, offset: 0x02a6 = 678 FAT32: ret: 000053a7, offset: 02a6 FAT32: entry: 0x53a7 = 21415, offset: 0x02a7 = 679 FAT32: ret: 000053a8, offset: 02a7 FAT32: entry: 0x53a8 = 21416, offset: 0x02a8 = 680 FAT32: ret: 000053a9, offset: 02a8 FAT32: entry: 0x53a9 = 21417, offset: 0x02a9 = 681 FAT32: ret: 000053aa, offset: 02a9 FAT32: entry: 0x53aa = 21418, offset: 0x02aa = 682 FAT32: ret: 000053ab, offset: 02aa FAT32: entry: 0x53ab = 21419, offset: 0x02ab = 683 FAT32: ret: 000053ac, offset: 02ab FAT32: entry: 0x53ac = 21420, offset: 0x02ac = 684 FAT32: ret: 000053ad, offset: 02ac FAT32: entry: 0x53ad = 21421, offset: 0x02ad = 685 FAT32: ret: 000053ae, offset: 02ad FAT32: entry: 0x53ae = 21422, offset: 0x02ae = 686 FAT32: ret: 000053af, offset: 02ae FAT32: entry: 0x53af = 21423, offset: 0x02af = 687 FAT32: ret: 000053b0, offset: 02af FAT32: entry: 0x53b0 = 21424, offset: 0x02b0 = 688 FAT32: ret: 000053b1, offset: 02b0 FAT32: entry: 0x53b1 = 21425, offset: 0x02b1 = 689 FAT32: ret: 000053b2, offset: 02b1 FAT32: entry: 0x53b2 = 21426, offset: 0x02b2 = 690 FAT32: ret: 000053b3, offset: 02b2 FAT32: entry: 0x53b3 = 21427, offset: 0x02b3 = 691 FAT32: ret: 000053b4, offset: 02b3 FAT32: entry: 0x53b4 = 21428, offset: 0x02b4 = 692 FAT32: ret: 000053b5, offset: 02b4 FAT32: entry: 0x53b5 = 21429, offset: 0x02b5 = 693 FAT32: ret: 000053b6, offset: 02b5 FAT32: entry: 0x53b6 = 21430, offset: 0x02b6 = 694 FAT32: ret: 000053b7, offset: 02b6 FAT32: entry: 0x53b7 = 21431, offset: 0x02b7 = 695 FAT32: ret: 000053b8, offset: 02b7 FAT32: entry: 0x53b8 = 21432, offset: 0x02b8 = 696 FAT32: ret: 000053b9, offset: 02b8 FAT32: entry: 0x53b9 = 21433, offset: 0x02b9 = 697 FAT32: ret: 000053ba, offset: 02b9 FAT32: entry: 0x53ba = 21434, offset: 0x02ba = 698 FAT32: ret: 000053bb, offset: 02ba FAT32: entry: 0x53bb = 21435, offset: 0x02bb = 699 FAT32: ret: 000053bc, offset: 02bb FAT32: entry: 0x53bc = 21436, offset: 0x02bc = 700 FAT32: ret: 000053bd, offset: 02bc FAT32: entry: 0x53bd = 21437, offset: 0x02bd = 701 FAT32: ret: 000053be, offset: 02bd FAT32: entry: 0x53be = 21438, offset: 0x02be = 702 FAT32: ret: 000053bf, offset: 02be FAT32: entry: 0x53bf = 21439, offset: 0x02bf = 703 FAT32: ret: 000053c0, offset: 02bf FAT32: entry: 0x53c0 = 21440, offset: 0x02c0 = 704 FAT32: ret: 000053c1, offset: 02c0 FAT32: entry: 0x53c1 = 21441, offset: 0x02c1 = 705 FAT32: ret: 000053c2, offset: 02c1 FAT32: entry: 0x53c2 = 21442, offset: 0x02c2 = 706 FAT32: ret: 000053c3, offset: 02c2 FAT32: entry: 0x53c3 = 21443, offset: 0x02c3 = 707 FAT32: ret: 000053c4, offset: 02c3 FAT32: entry: 0x53c4 = 21444, offset: 0x02c4 = 708 FAT32: ret: 000053c5, offset: 02c4 FAT32: entry: 0x53c5 = 21445, offset: 0x02c5 = 709 FAT32: ret: 000053c6, offset: 02c5 FAT32: entry: 0x53c6 = 21446, offset: 0x02c6 = 710 FAT32: ret: 000053c7, offset: 02c6 FAT32: entry: 0x53c7 = 21447, offset: 0x02c7 = 711 FAT32: ret: 000053c8, offset: 02c7 FAT32: entry: 0x53c8 = 21448, offset: 0x02c8 = 712 FAT32: ret: 000053c9, offset: 02c8 FAT32: entry: 0x53c9 = 21449, offset: 0x02c9 = 713 FAT32: ret: 000053ca, offset: 02c9 FAT32: entry: 0x53ca = 21450, offset: 0x02ca = 714 FAT32: ret: 000053cb, offset: 02ca FAT32: entry: 0x53cb = 21451, offset: 0x02cb = 715 FAT32: ret: 000053cc, offset: 02cb FAT32: entry: 0x53cc = 21452, offset: 0x02cc = 716 FAT32: ret: 000053cd, offset: 02cc FAT32: entry: 0x53cd = 21453, offset: 0x02cd = 717 FAT32: ret: 000053ce, offset: 02cd FAT32: entry: 0x53ce = 21454, offset: 0x02ce = 718 FAT32: ret: 000053cf, offset: 02ce FAT32: entry: 0x53cf = 21455, offset: 0x02cf = 719 FAT32: ret: 000053d0, offset: 02cf FAT32: entry: 0x53d0 = 21456, offset: 0x02d0 = 720 FAT32: ret: 000053d1, offset: 02d0 FAT32: entry: 0x53d1 = 21457, offset: 0x02d1 = 721 FAT32: ret: 000053d2, offset: 02d1 FAT32: entry: 0x53d2 = 21458, offset: 0x02d2 = 722 FAT32: ret: 000053d3, offset: 02d2 FAT32: entry: 0x53d3 = 21459, offset: 0x02d3 = 723 FAT32: ret: 000053d4, offset: 02d3 FAT32: entry: 0x53d4 = 21460, offset: 0x02d4 = 724 FAT32: ret: 000053d5, offset: 02d4 FAT32: entry: 0x53d5 = 21461, offset: 0x02d5 = 725 FAT32: ret: 000053d6, offset: 02d5 FAT32: entry: 0x53d6 = 21462, offset: 0x02d6 = 726 FAT32: ret: 000053d7, offset: 02d6 FAT32: entry: 0x53d7 = 21463, offset: 0x02d7 = 727 FAT32: ret: 000053d8, offset: 02d7 FAT32: entry: 0x53d8 = 21464, offset: 0x02d8 = 728 FAT32: ret: 000053d9, offset: 02d8 FAT32: entry: 0x53d9 = 21465, offset: 0x02d9 = 729 FAT32: ret: 000053da, offset: 02d9 FAT32: entry: 0x53da = 21466, offset: 0x02da = 730 FAT32: ret: 000053db, offset: 02da FAT32: entry: 0x53db = 21467, offset: 0x02db = 731 FAT32: ret: 000053dc, offset: 02db FAT32: entry: 0x53dc = 21468, offset: 0x02dc = 732 FAT32: ret: 000053dd, offset: 02dc FAT32: entry: 0x53dd = 21469, offset: 0x02dd = 733 FAT32: ret: 000053de, offset: 02dd FAT32: entry: 0x53de = 21470, offset: 0x02de = 734 FAT32: ret: 000053df, offset: 02de FAT32: entry: 0x53df = 21471, offset: 0x02df = 735 FAT32: ret: 000053e0, offset: 02df FAT32: entry: 0x53e0 = 21472, offset: 0x02e0 = 736 FAT32: ret: 000053e1, offset: 02e0 FAT32: entry: 0x53e1 = 21473, offset: 0x02e1 = 737 FAT32: ret: 000053e2, offset: 02e1 FAT32: entry: 0x53e2 = 21474, offset: 0x02e2 = 738 FAT32: ret: 000053e3, offset: 02e2 FAT32: entry: 0x53e3 = 21475, offset: 0x02e3 = 739 FAT32: ret: 000053e4, offset: 02e3 FAT32: entry: 0x53e4 = 21476, offset: 0x02e4 = 740 FAT32: ret: 000053e5, offset: 02e4 FAT32: entry: 0x53e5 = 21477, offset: 0x02e5 = 741 FAT32: ret: 000053e6, offset: 02e5 FAT32: entry: 0x53e6 = 21478, offset: 0x02e6 = 742 FAT32: ret: 000053e7, offset: 02e6 FAT32: entry: 0x53e7 = 21479, offset: 0x02e7 = 743 FAT32: ret: 000053e8, offset: 02e7 FAT32: entry: 0x53e8 = 21480, offset: 0x02e8 = 744 FAT32: ret: 000053e9, offset: 02e8 FAT32: entry: 0x53e9 = 21481, offset: 0x02e9 = 745 FAT32: ret: 000053ea, offset: 02e9 FAT32: entry: 0x53ea = 21482, offset: 0x02ea = 746 FAT32: ret: 000053eb, offset: 02ea FAT32: entry: 0x53eb = 21483, offset: 0x02eb = 747 FAT32: ret: 000053ec, offset: 02eb FAT32: entry: 0x53ec = 21484, offset: 0x02ec = 748 FAT32: ret: 000053ed, offset: 02ec FAT32: entry: 0x53ed = 21485, offset: 0x02ed = 749 FAT32: ret: 000053ee, offset: 02ed FAT32: entry: 0x53ee = 21486, offset: 0x02ee = 750 FAT32: ret: 000053ef, offset: 02ee FAT32: entry: 0x53ef = 21487, offset: 0x02ef = 751 FAT32: ret: 000053f0, offset: 02ef FAT32: entry: 0x53f0 = 21488, offset: 0x02f0 = 752 FAT32: ret: 000053f1, offset: 02f0 FAT32: entry: 0x53f1 = 21489, offset: 0x02f1 = 753 FAT32: ret: 000053f2, offset: 02f1 FAT32: entry: 0x53f2 = 21490, offset: 0x02f2 = 754 FAT32: ret: 000053f3, offset: 02f2 FAT32: entry: 0x53f3 = 21491, offset: 0x02f3 = 755 FAT32: ret: 000053f4, offset: 02f3 FAT32: entry: 0x53f4 = 21492, offset: 0x02f4 = 756 FAT32: ret: 000053f5, offset: 02f4 FAT32: entry: 0x53f5 = 21493, offset: 0x02f5 = 757 FAT32: ret: 000053f6, offset: 02f5 FAT32: entry: 0x53f6 = 21494, offset: 0x02f6 = 758 FAT32: ret: 000053f7, offset: 02f6 FAT32: entry: 0x53f7 = 21495, offset: 0x02f7 = 759 FAT32: ret: 000053f8, offset: 02f7 FAT32: entry: 0x53f8 = 21496, offset: 0x02f8 = 760 FAT32: ret: 000053f9, offset: 02f8 FAT32: entry: 0x53f9 = 21497, offset: 0x02f9 = 761 FAT32: ret: 000053fa, offset: 02f9 FAT32: entry: 0x53fa = 21498, offset: 0x02fa = 762 FAT32: ret: 000053fb, offset: 02fa FAT32: entry: 0x53fb = 21499, offset: 0x02fb = 763 FAT32: ret: 000053fc, offset: 02fb FAT32: entry: 0x53fc = 21500, offset: 0x02fc = 764 FAT32: ret: 000053fd, offset: 02fc FAT32: entry: 0x53fd = 21501, offset: 0x02fd = 765 FAT32: ret: 000053fe, offset: 02fd FAT32: entry: 0x53fe = 21502, offset: 0x02fe = 766 FAT32: ret: 000053ff, offset: 02fe FAT32: entry: 0x53ff = 21503, offset: 0x02ff = 767 FAT32: ret: 00005400, offset: 02ff FAT32: entry: 0x5400 = 21504, offset: 0x0000 = 0 FAT32: ret: 00005401, offset: 0000 FAT32: entry: 0x5401 = 21505, offset: 0x0001 = 1 FAT32: ret: 00005402, offset: 0001 FAT32: entry: 0x5402 = 21506, offset: 0x0002 = 2 FAT32: ret: 00005403, offset: 0002 FAT32: entry: 0x5403 = 21507, offset: 0x0003 = 3 FAT32: ret: 00005404, offset: 0003 FAT32: entry: 0x5404 = 21508, offset: 0x0004 = 4 FAT32: ret: 00005405, offset: 0004 FAT32: entry: 0x5405 = 21509, offset: 0x0005 = 5 FAT32: ret: 00005406, offset: 0005 FAT32: entry: 0x5406 = 21510, offset: 0x0006 = 6 FAT32: ret: 00005407, offset: 0006 FAT32: entry: 0x5407 = 21511, offset: 0x0007 = 7 FAT32: ret: 00005408, offset: 0007 FAT32: entry: 0x5408 = 21512, offset: 0x0008 = 8 FAT32: ret: 00005409, offset: 0008 FAT32: entry: 0x5409 = 21513, offset: 0x0009 = 9 FAT32: ret: 0000540a, offset: 0009 FAT32: entry: 0x540a = 21514, offset: 0x000a = 10 FAT32: ret: 0000540b, offset: 000a FAT32: entry: 0x540b = 21515, offset: 0x000b = 11 FAT32: ret: 0000540c, offset: 000b FAT32: entry: 0x540c = 21516, offset: 0x000c = 12 FAT32: ret: 0000540d, offset: 000c FAT32: entry: 0x540d = 21517, offset: 0x000d = 13 FAT32: ret: 0000540e, offset: 000d FAT32: entry: 0x540e = 21518, offset: 0x000e = 14 FAT32: ret: 0000540f, offset: 000e FAT32: entry: 0x540f = 21519, offset: 0x000f = 15 FAT32: ret: 00005410, offset: 000f FAT32: entry: 0x5410 = 21520, offset: 0x0010 = 16 FAT32: ret: 00005411, offset: 0010 FAT32: entry: 0x5411 = 21521, offset: 0x0011 = 17 FAT32: ret: 00005412, offset: 0011 FAT32: entry: 0x5412 = 21522, offset: 0x0012 = 18 FAT32: ret: 00005413, offset: 0012 FAT32: entry: 0x5413 = 21523, offset: 0x0013 = 19 FAT32: ret: 00005414, offset: 0013 FAT32: entry: 0x5414 = 21524, offset: 0x0014 = 20 FAT32: ret: 00005415, offset: 0014 FAT32: entry: 0x5415 = 21525, offset: 0x0015 = 21 FAT32: ret: 00005416, offset: 0015 FAT32: entry: 0x5416 = 21526, offset: 0x0016 = 22 FAT32: ret: 00005417, offset: 0016 FAT32: entry: 0x5417 = 21527, offset: 0x0017 = 23 FAT32: ret: 00005418, offset: 0017 FAT32: entry: 0x5418 = 21528, offset: 0x0018 = 24 FAT32: ret: 00005419, offset: 0018 FAT32: entry: 0x5419 = 21529, offset: 0x0019 = 25 FAT32: ret: 0000541a, offset: 0019 FAT32: entry: 0x541a = 21530, offset: 0x001a = 26 FAT32: ret: 0000541b, offset: 001a FAT32: entry: 0x541b = 21531, offset: 0x001b = 27 FAT32: ret: 0000541c, offset: 001b FAT32: entry: 0x541c = 21532, offset: 0x001c = 28 FAT32: ret: 0000541d, offset: 001c FAT32: entry: 0x541d = 21533, offset: 0x001d = 29 FAT32: ret: 0000541e, offset: 001d FAT32: entry: 0x541e = 21534, offset: 0x001e = 30 FAT32: ret: 0000541f, offset: 001e FAT32: entry: 0x541f = 21535, offset: 0x001f = 31 FAT32: ret: 00005420, offset: 001f FAT32: entry: 0x5420 = 21536, offset: 0x0020 = 32 FAT32: ret: 00005421, offset: 0020 FAT32: entry: 0x5421 = 21537, offset: 0x0021 = 33 FAT32: ret: 00005422, offset: 0021 FAT32: entry: 0x5422 = 21538, offset: 0x0022 = 34 FAT32: ret: 00005423, offset: 0022 FAT32: entry: 0x5423 = 21539, offset: 0x0023 = 35 FAT32: ret: 00005424, offset: 0023 FAT32: entry: 0x5424 = 21540, offset: 0x0024 = 36 FAT32: ret: 00005425, offset: 0024 FAT32: entry: 0x5425 = 21541, offset: 0x0025 = 37 FAT32: ret: 00005426, offset: 0025 FAT32: entry: 0x5426 = 21542, offset: 0x0026 = 38 FAT32: ret: 00005427, offset: 0026 FAT32: entry: 0x5427 = 21543, offset: 0x0027 = 39 FAT32: ret: 00005428, offset: 0027 FAT32: entry: 0x5428 = 21544, offset: 0x0028 = 40 FAT32: ret: 00005429, offset: 0028 FAT32: entry: 0x5429 = 21545, offset: 0x0029 = 41 FAT32: ret: 0000542a, offset: 0029 FAT32: entry: 0x542a = 21546, offset: 0x002a = 42 FAT32: ret: 0000542b, offset: 002a FAT32: entry: 0x542b = 21547, offset: 0x002b = 43 FAT32: ret: 0000542c, offset: 002b FAT32: entry: 0x542c = 21548, offset: 0x002c = 44 FAT32: ret: 0000542d, offset: 002c FAT32: entry: 0x542d = 21549, offset: 0x002d = 45 FAT32: ret: 0000542e, offset: 002d FAT32: entry: 0x542e = 21550, offset: 0x002e = 46 FAT32: ret: 0000542f, offset: 002e FAT32: entry: 0x542f = 21551, offset: 0x002f = 47 FAT32: ret: 00005430, offset: 002f FAT32: entry: 0x5430 = 21552, offset: 0x0030 = 48 FAT32: ret: 00005431, offset: 0030 FAT32: entry: 0x5431 = 21553, offset: 0x0031 = 49 FAT32: ret: 00005432, offset: 0031 FAT32: entry: 0x5432 = 21554, offset: 0x0032 = 50 FAT32: ret: 00005433, offset: 0032 FAT32: entry: 0x5433 = 21555, offset: 0x0033 = 51 FAT32: ret: 00005434, offset: 0033 FAT32: entry: 0x5434 = 21556, offset: 0x0034 = 52 FAT32: ret: 00005435, offset: 0034 FAT32: entry: 0x5435 = 21557, offset: 0x0035 = 53 FAT32: ret: 00005436, offset: 0035 FAT32: entry: 0x5436 = 21558, offset: 0x0036 = 54 FAT32: ret: 00005437, offset: 0036 FAT32: entry: 0x5437 = 21559, offset: 0x0037 = 55 FAT32: ret: 00005438, offset: 0037 FAT32: entry: 0x5438 = 21560, offset: 0x0038 = 56 FAT32: ret: 00005439, offset: 0038 FAT32: entry: 0x5439 = 21561, offset: 0x0039 = 57 FAT32: ret: 0000543a, offset: 0039 FAT32: entry: 0x543a = 21562, offset: 0x003a = 58 FAT32: ret: 0000543b, offset: 003a FAT32: entry: 0x543b = 21563, offset: 0x003b = 59 FAT32: ret: 0000543c, offset: 003b FAT32: entry: 0x543c = 21564, offset: 0x003c = 60 FAT32: ret: 0000543d, offset: 003c FAT32: entry: 0x543d = 21565, offset: 0x003d = 61 FAT32: ret: 0000543e, offset: 003d FAT32: entry: 0x543e = 21566, offset: 0x003e = 62 FAT32: ret: 0000543f, offset: 003e FAT32: entry: 0x543f = 21567, offset: 0x003f = 63 FAT32: ret: 00005440, offset: 003f FAT32: entry: 0x5440 = 21568, offset: 0x0040 = 64 FAT32: ret: 00005441, offset: 0040 FAT32: entry: 0x5441 = 21569, offset: 0x0041 = 65 FAT32: ret: 00005442, offset: 0041 FAT32: entry: 0x5442 = 21570, offset: 0x0042 = 66 FAT32: ret: 00005443, offset: 0042 FAT32: entry: 0x5443 = 21571, offset: 0x0043 = 67 FAT32: ret: 00005444, offset: 0043 FAT32: entry: 0x5444 = 21572, offset: 0x0044 = 68 FAT32: ret: 00005445, offset: 0044 FAT32: entry: 0x5445 = 21573, offset: 0x0045 = 69 FAT32: ret: 00005446, offset: 0045 FAT32: entry: 0x5446 = 21574, offset: 0x0046 = 70 FAT32: ret: 00005447, offset: 0046 FAT32: entry: 0x5447 = 21575, offset: 0x0047 = 71 FAT32: ret: 00005448, offset: 0047 FAT32: entry: 0x5448 = 21576, offset: 0x0048 = 72 FAT32: ret: 00005449, offset: 0048 FAT32: entry: 0x5449 = 21577, offset: 0x0049 = 73 FAT32: ret: 0000544a, offset: 0049 FAT32: entry: 0x544a = 21578, offset: 0x004a = 74 FAT32: ret: 0000544b, offset: 004a FAT32: entry: 0x544b = 21579, offset: 0x004b = 75 FAT32: ret: 0000544c, offset: 004b FAT32: entry: 0x544c = 21580, offset: 0x004c = 76 FAT32: ret: 0000544d, offset: 004c FAT32: entry: 0x544d = 21581, offset: 0x004d = 77 FAT32: ret: 0000544e, offset: 004d FAT32: entry: 0x544e = 21582, offset: 0x004e = 78 FAT32: ret: 0000544f, offset: 004e FAT32: entry: 0x544f = 21583, offset: 0x004f = 79 FAT32: ret: 00005450, offset: 004f FAT32: entry: 0x5450 = 21584, offset: 0x0050 = 80 FAT32: ret: 00005451, offset: 0050 FAT32: entry: 0x5451 = 21585, offset: 0x0051 = 81 FAT32: ret: 00005452, offset: 0051 FAT32: entry: 0x5452 = 21586, offset: 0x0052 = 82 FAT32: ret: 00005453, offset: 0052 FAT32: entry: 0x5453 = 21587, offset: 0x0053 = 83 FAT32: ret: 00005454, offset: 0053 FAT32: entry: 0x5454 = 21588, offset: 0x0054 = 84 FAT32: ret: 00005455, offset: 0054 FAT32: entry: 0x5455 = 21589, offset: 0x0055 = 85 FAT32: ret: 00005456, offset: 0055 FAT32: entry: 0x5456 = 21590, offset: 0x0056 = 86 FAT32: ret: 00005457, offset: 0056 FAT32: entry: 0x5457 = 21591, offset: 0x0057 = 87 FAT32: ret: 00005458, offset: 0057 FAT32: entry: 0x5458 = 21592, offset: 0x0058 = 88 FAT32: ret: 00005459, offset: 0058 FAT32: entry: 0x5459 = 21593, offset: 0x0059 = 89 FAT32: ret: 0000545a, offset: 0059 FAT32: entry: 0x545a = 21594, offset: 0x005a = 90 FAT32: ret: 0000545b, offset: 005a FAT32: entry: 0x545b = 21595, offset: 0x005b = 91 FAT32: ret: 0000545c, offset: 005b FAT32: entry: 0x545c = 21596, offset: 0x005c = 92 FAT32: ret: 0000545d, offset: 005c FAT32: entry: 0x545d = 21597, offset: 0x005d = 93 FAT32: ret: 0000545e, offset: 005d FAT32: entry: 0x545e = 21598, offset: 0x005e = 94 FAT32: ret: 0000545f, offset: 005e FAT32: entry: 0x545f = 21599, offset: 0x005f = 95 FAT32: ret: 00005460, offset: 005f FAT32: entry: 0x5460 = 21600, offset: 0x0060 = 96 FAT32: ret: 00005461, offset: 0060 FAT32: entry: 0x5461 = 21601, offset: 0x0061 = 97 FAT32: ret: 00005462, offset: 0061 FAT32: entry: 0x5462 = 21602, offset: 0x0062 = 98 FAT32: ret: 00005463, offset: 0062 FAT32: entry: 0x5463 = 21603, offset: 0x0063 = 99 FAT32: ret: 00005464, offset: 0063 FAT32: entry: 0x5464 = 21604, offset: 0x0064 = 100 FAT32: ret: 00005465, offset: 0064 FAT32: entry: 0x5465 = 21605, offset: 0x0065 = 101 FAT32: ret: 00005466, offset: 0065 FAT32: entry: 0x5466 = 21606, offset: 0x0066 = 102 FAT32: ret: 00005467, offset: 0066 FAT32: entry: 0x5467 = 21607, offset: 0x0067 = 103 FAT32: ret: 00005468, offset: 0067 FAT32: entry: 0x5468 = 21608, offset: 0x0068 = 104 FAT32: ret: 00005469, offset: 0068 FAT32: entry: 0x5469 = 21609, offset: 0x0069 = 105 FAT32: ret: 0000546a, offset: 0069 FAT32: entry: 0x546a = 21610, offset: 0x006a = 106 FAT32: ret: 0000546b, offset: 006a FAT32: entry: 0x546b = 21611, offset: 0x006b = 107 FAT32: ret: 0000546c, offset: 006b FAT32: entry: 0x546c = 21612, offset: 0x006c = 108 FAT32: ret: 0000546d, offset: 006c FAT32: entry: 0x546d = 21613, offset: 0x006d = 109 FAT32: ret: 0000546e, offset: 006d FAT32: entry: 0x546e = 21614, offset: 0x006e = 110 FAT32: ret: 0000546f, offset: 006e FAT32: entry: 0x546f = 21615, offset: 0x006f = 111 FAT32: ret: 00005470, offset: 006f FAT32: entry: 0x5470 = 21616, offset: 0x0070 = 112 FAT32: ret: 00005471, offset: 0070 FAT32: entry: 0x5471 = 21617, offset: 0x0071 = 113 FAT32: ret: 00005472, offset: 0071 FAT32: entry: 0x5472 = 21618, offset: 0x0072 = 114 FAT32: ret: 00005473, offset: 0072 FAT32: entry: 0x5473 = 21619, offset: 0x0073 = 115 FAT32: ret: 00005474, offset: 0073 FAT32: entry: 0x5474 = 21620, offset: 0x0074 = 116 FAT32: ret: 00005475, offset: 0074 FAT32: entry: 0x5475 = 21621, offset: 0x0075 = 117 FAT32: ret: 00005476, offset: 0075 FAT32: entry: 0x5476 = 21622, offset: 0x0076 = 118 FAT32: ret: 00005477, offset: 0076 FAT32: entry: 0x5477 = 21623, offset: 0x0077 = 119 FAT32: ret: 00005478, offset: 0077 FAT32: entry: 0x5478 = 21624, offset: 0x0078 = 120 FAT32: ret: 00005479, offset: 0078 FAT32: entry: 0x5479 = 21625, offset: 0x0079 = 121 FAT32: ret: 0000547a, offset: 0079 FAT32: entry: 0x547a = 21626, offset: 0x007a = 122 FAT32: ret: 0000547b, offset: 007a FAT32: entry: 0x547b = 21627, offset: 0x007b = 123 FAT32: ret: 0000547c, offset: 007b FAT32: entry: 0x547c = 21628, offset: 0x007c = 124 FAT32: ret: 0000547d, offset: 007c FAT32: entry: 0x547d = 21629, offset: 0x007d = 125 FAT32: ret: 0000547e, offset: 007d FAT32: entry: 0x547e = 21630, offset: 0x007e = 126 FAT32: ret: 0000547f, offset: 007e FAT32: entry: 0x547f = 21631, offset: 0x007f = 127 FAT32: ret: 00005480, offset: 007f FAT32: entry: 0x5480 = 21632, offset: 0x0080 = 128 FAT32: ret: 00005481, offset: 0080 FAT32: entry: 0x5481 = 21633, offset: 0x0081 = 129 FAT32: ret: 00005482, offset: 0081 FAT32: entry: 0x5482 = 21634, offset: 0x0082 = 130 FAT32: ret: 00005483, offset: 0082 FAT32: entry: 0x5483 = 21635, offset: 0x0083 = 131 FAT32: ret: 00005484, offset: 0083 FAT32: entry: 0x5484 = 21636, offset: 0x0084 = 132 FAT32: ret: 00005485, offset: 0084 FAT32: entry: 0x5485 = 21637, offset: 0x0085 = 133 FAT32: ret: 00005486, offset: 0085 FAT32: entry: 0x5486 = 21638, offset: 0x0086 = 134 FAT32: ret: 00005487, offset: 0086 FAT32: entry: 0x5487 = 21639, offset: 0x0087 = 135 FAT32: ret: 00005488, offset: 0087 FAT32: entry: 0x5488 = 21640, offset: 0x0088 = 136 FAT32: ret: 00005489, offset: 0088 FAT32: entry: 0x5489 = 21641, offset: 0x0089 = 137 FAT32: ret: 0000548a, offset: 0089 FAT32: entry: 0x548a = 21642, offset: 0x008a = 138 FAT32: ret: 0000548b, offset: 008a FAT32: entry: 0x548b = 21643, offset: 0x008b = 139 FAT32: ret: 0000548c, offset: 008b FAT32: entry: 0x548c = 21644, offset: 0x008c = 140 FAT32: ret: 0000548d, offset: 008c FAT32: entry: 0x548d = 21645, offset: 0x008d = 141 FAT32: ret: 0000548e, offset: 008d FAT32: entry: 0x548e = 21646, offset: 0x008e = 142 FAT32: ret: 0000548f, offset: 008e FAT32: entry: 0x548f = 21647, offset: 0x008f = 143 FAT32: ret: 00005490, offset: 008f FAT32: entry: 0x5490 = 21648, offset: 0x0090 = 144 FAT32: ret: 00005491, offset: 0090 FAT32: entry: 0x5491 = 21649, offset: 0x0091 = 145 FAT32: ret: 00005492, offset: 0091 FAT32: entry: 0x5492 = 21650, offset: 0x0092 = 146 FAT32: ret: 00005493, offset: 0092 FAT32: entry: 0x5493 = 21651, offset: 0x0093 = 147 FAT32: ret: 00005494, offset: 0093 FAT32: entry: 0x5494 = 21652, offset: 0x0094 = 148 FAT32: ret: 00005495, offset: 0094 FAT32: entry: 0x5495 = 21653, offset: 0x0095 = 149 FAT32: ret: 00005496, offset: 0095 FAT32: entry: 0x5496 = 21654, offset: 0x0096 = 150 FAT32: ret: 00005497, offset: 0096 FAT32: entry: 0x5497 = 21655, offset: 0x0097 = 151 FAT32: ret: 00005498, offset: 0097 FAT32: entry: 0x5498 = 21656, offset: 0x0098 = 152 FAT32: ret: 00005499, offset: 0098 FAT32: entry: 0x5499 = 21657, offset: 0x0099 = 153 FAT32: ret: 0000549a, offset: 0099 FAT32: entry: 0x549a = 21658, offset: 0x009a = 154 FAT32: ret: 0000549b, offset: 009a FAT32: entry: 0x549b = 21659, offset: 0x009b = 155 FAT32: ret: 0000549c, offset: 009b FAT32: entry: 0x549c = 21660, offset: 0x009c = 156 FAT32: ret: 0000549d, offset: 009c FAT32: entry: 0x549d = 21661, offset: 0x009d = 157 FAT32: ret: 0000549e, offset: 009d FAT32: entry: 0x549e = 21662, offset: 0x009e = 158 FAT32: ret: 0000549f, offset: 009e FAT32: entry: 0x549f = 21663, offset: 0x009f = 159 FAT32: ret: 000054a0, offset: 009f FAT32: entry: 0x54a0 = 21664, offset: 0x00a0 = 160 FAT32: ret: 000054a1, offset: 00a0 FAT32: entry: 0x54a1 = 21665, offset: 0x00a1 = 161 FAT32: ret: 000054a2, offset: 00a1 FAT32: entry: 0x54a2 = 21666, offset: 0x00a2 = 162 FAT32: ret: 000054a3, offset: 00a2 FAT32: entry: 0x54a3 = 21667, offset: 0x00a3 = 163 FAT32: ret: 000054a4, offset: 00a3 FAT32: entry: 0x54a4 = 21668, offset: 0x00a4 = 164 FAT32: ret: 000054a5, offset: 00a4 FAT32: entry: 0x54a5 = 21669, offset: 0x00a5 = 165 FAT32: ret: 000054a6, offset: 00a5 FAT32: entry: 0x54a6 = 21670, offset: 0x00a6 = 166 FAT32: ret: 000054a7, offset: 00a6 FAT32: entry: 0x54a7 = 21671, offset: 0x00a7 = 167 FAT32: ret: 000054a8, offset: 00a7 FAT32: entry: 0x54a8 = 21672, offset: 0x00a8 = 168 FAT32: ret: 000054a9, offset: 00a8 FAT32: entry: 0x54a9 = 21673, offset: 0x00a9 = 169 FAT32: ret: 000054aa, offset: 00a9 FAT32: entry: 0x54aa = 21674, offset: 0x00aa = 170 FAT32: ret: 000054ab, offset: 00aa FAT32: entry: 0x54ab = 21675, offset: 0x00ab = 171 FAT32: ret: 000054ac, offset: 00ab FAT32: entry: 0x54ac = 21676, offset: 0x00ac = 172 FAT32: ret: 000054ad, offset: 00ac FAT32: entry: 0x54ad = 21677, offset: 0x00ad = 173 FAT32: ret: 000054ae, offset: 00ad FAT32: entry: 0x54ae = 21678, offset: 0x00ae = 174 FAT32: ret: 000054af, offset: 00ae FAT32: entry: 0x54af = 21679, offset: 0x00af = 175 FAT32: ret: 000054b0, offset: 00af FAT32: entry: 0x54b0 = 21680, offset: 0x00b0 = 176 FAT32: ret: 000054b1, offset: 00b0 FAT32: entry: 0x54b1 = 21681, offset: 0x00b1 = 177 FAT32: ret: 000054b2, offset: 00b1 FAT32: entry: 0x54b2 = 21682, offset: 0x00b2 = 178 FAT32: ret: 000054b3, offset: 00b2 FAT32: entry: 0x54b3 = 21683, offset: 0x00b3 = 179 FAT32: ret: 000054b4, offset: 00b3 FAT32: entry: 0x54b4 = 21684, offset: 0x00b4 = 180 FAT32: ret: 000054b5, offset: 00b4 FAT32: entry: 0x54b5 = 21685, offset: 0x00b5 = 181 FAT32: ret: 000054b6, offset: 00b5 FAT32: entry: 0x54b6 = 21686, offset: 0x00b6 = 182 FAT32: ret: 000054b7, offset: 00b6 FAT32: entry: 0x54b7 = 21687, offset: 0x00b7 = 183 FAT32: ret: 000054b8, offset: 00b7 FAT32: entry: 0x54b8 = 21688, offset: 0x00b8 = 184 FAT32: ret: 000054b9, offset: 00b8 FAT32: entry: 0x54b9 = 21689, offset: 0x00b9 = 185 FAT32: ret: 000054ba, offset: 00b9 FAT32: entry: 0x54ba = 21690, offset: 0x00ba = 186 FAT32: ret: 000054bb, offset: 00ba FAT32: entry: 0x54bb = 21691, offset: 0x00bb = 187 FAT32: ret: 000054bc, offset: 00bb FAT32: entry: 0x54bc = 21692, offset: 0x00bc = 188 FAT32: ret: 000054bd, offset: 00bc FAT32: entry: 0x54bd = 21693, offset: 0x00bd = 189 FAT32: ret: 000054be, offset: 00bd FAT32: entry: 0x54be = 21694, offset: 0x00be = 190 FAT32: ret: 000054bf, offset: 00be FAT32: entry: 0x54bf = 21695, offset: 0x00bf = 191 FAT32: ret: 000054c0, offset: 00bf FAT32: entry: 0x54c0 = 21696, offset: 0x00c0 = 192 FAT32: ret: 000054c1, offset: 00c0 FAT32: entry: 0x54c1 = 21697, offset: 0x00c1 = 193 FAT32: ret: 000054c2, offset: 00c1 FAT32: entry: 0x54c2 = 21698, offset: 0x00c2 = 194 FAT32: ret: 000054c3, offset: 00c2 FAT32: entry: 0x54c3 = 21699, offset: 0x00c3 = 195 FAT32: ret: 000054c4, offset: 00c3 FAT32: entry: 0x54c4 = 21700, offset: 0x00c4 = 196 FAT32: ret: 000054c5, offset: 00c4 FAT32: entry: 0x54c5 = 21701, offset: 0x00c5 = 197 FAT32: ret: 000054c6, offset: 00c5 FAT32: entry: 0x54c6 = 21702, offset: 0x00c6 = 198 FAT32: ret: 000054c7, offset: 00c6 FAT32: entry: 0x54c7 = 21703, offset: 0x00c7 = 199 FAT32: ret: 000054c8, offset: 00c7 FAT32: entry: 0x54c8 = 21704, offset: 0x00c8 = 200 FAT32: ret: 000054c9, offset: 00c8 FAT32: entry: 0x54c9 = 21705, offset: 0x00c9 = 201 FAT32: ret: 000054ca, offset: 00c9 FAT32: entry: 0x54ca = 21706, offset: 0x00ca = 202 FAT32: ret: 000054cb, offset: 00ca FAT32: entry: 0x54cb = 21707, offset: 0x00cb = 203 FAT32: ret: 000054cc, offset: 00cb FAT32: entry: 0x54cc = 21708, offset: 0x00cc = 204 FAT32: ret: 000054cd, offset: 00cc FAT32: entry: 0x54cd = 21709, offset: 0x00cd = 205 FAT32: ret: 000054ce, offset: 00cd FAT32: entry: 0x54ce = 21710, offset: 0x00ce = 206 FAT32: ret: 000054cf, offset: 00ce FAT32: entry: 0x54cf = 21711, offset: 0x00cf = 207 FAT32: ret: 000054d0, offset: 00cf FAT32: entry: 0x54d0 = 21712, offset: 0x00d0 = 208 FAT32: ret: 000054d1, offset: 00d0 FAT32: entry: 0x54d1 = 21713, offset: 0x00d1 = 209 FAT32: ret: 000054d2, offset: 00d1 FAT32: entry: 0x54d2 = 21714, offset: 0x00d2 = 210 FAT32: ret: 000054d3, offset: 00d2 FAT32: entry: 0x54d3 = 21715, offset: 0x00d3 = 211 FAT32: ret: 000054d4, offset: 00d3 FAT32: entry: 0x54d4 = 21716, offset: 0x00d4 = 212 FAT32: ret: 000054d5, offset: 00d4 FAT32: entry: 0x54d5 = 21717, offset: 0x00d5 = 213 FAT32: ret: 000054d6, offset: 00d5 FAT32: entry: 0x54d6 = 21718, offset: 0x00d6 = 214 FAT32: ret: 000054d7, offset: 00d6 FAT32: entry: 0x54d7 = 21719, offset: 0x00d7 = 215 FAT32: ret: 000054d8, offset: 00d7 FAT32: entry: 0x54d8 = 21720, offset: 0x00d8 = 216 FAT32: ret: 000054d9, offset: 00d8 FAT32: entry: 0x54d9 = 21721, offset: 0x00d9 = 217 FAT32: ret: 000054da, offset: 00d9 FAT32: entry: 0x54da = 21722, offset: 0x00da = 218 FAT32: ret: 000054db, offset: 00da FAT32: entry: 0x54db = 21723, offset: 0x00db = 219 FAT32: ret: 000054dc, offset: 00db FAT32: entry: 0x54dc = 21724, offset: 0x00dc = 220 FAT32: ret: 000054dd, offset: 00dc FAT32: entry: 0x54dd = 21725, offset: 0x00dd = 221 FAT32: ret: 000054de, offset: 00dd FAT32: entry: 0x54de = 21726, offset: 0x00de = 222 FAT32: ret: 000054df, offset: 00de FAT32: entry: 0x54df = 21727, offset: 0x00df = 223 FAT32: ret: 000054e0, offset: 00df FAT32: entry: 0x54e0 = 21728, offset: 0x00e0 = 224 FAT32: ret: 000054e1, offset: 00e0 FAT32: entry: 0x54e1 = 21729, offset: 0x00e1 = 225 FAT32: ret: 000054e2, offset: 00e1 FAT32: entry: 0x54e2 = 21730, offset: 0x00e2 = 226 FAT32: ret: 000054e3, offset: 00e2 FAT32: entry: 0x54e3 = 21731, offset: 0x00e3 = 227 FAT32: ret: 000054e4, offset: 00e3 FAT32: entry: 0x54e4 = 21732, offset: 0x00e4 = 228 FAT32: ret: 000054e5, offset: 00e4 FAT32: entry: 0x54e5 = 21733, offset: 0x00e5 = 229 FAT32: ret: 000054e6, offset: 00e5 FAT32: entry: 0x54e6 = 21734, offset: 0x00e6 = 230 FAT32: ret: 000054e7, offset: 00e6 FAT32: entry: 0x54e7 = 21735, offset: 0x00e7 = 231 FAT32: ret: 000054e8, offset: 00e7 FAT32: entry: 0x54e8 = 21736, offset: 0x00e8 = 232 FAT32: ret: 000054e9, offset: 00e8 FAT32: entry: 0x54e9 = 21737, offset: 0x00e9 = 233 FAT32: ret: 000054ea, offset: 00e9 FAT32: entry: 0x54ea = 21738, offset: 0x00ea = 234 FAT32: ret: 000054eb, offset: 00ea FAT32: entry: 0x54eb = 21739, offset: 0x00eb = 235 FAT32: ret: 000054ec, offset: 00eb FAT32: entry: 0x54ec = 21740, offset: 0x00ec = 236 FAT32: ret: 000054ed, offset: 00ec FAT32: entry: 0x54ed = 21741, offset: 0x00ed = 237 FAT32: ret: 000054ee, offset: 00ed FAT32: entry: 0x54ee = 21742, offset: 0x00ee = 238 FAT32: ret: 000054ef, offset: 00ee FAT32: entry: 0x54ef = 21743, offset: 0x00ef = 239 FAT32: ret: 000054f0, offset: 00ef FAT32: entry: 0x54f0 = 21744, offset: 0x00f0 = 240 FAT32: ret: 000054f1, offset: 00f0 FAT32: entry: 0x54f1 = 21745, offset: 0x00f1 = 241 FAT32: ret: 000054f2, offset: 00f1 FAT32: entry: 0x54f2 = 21746, offset: 0x00f2 = 242 FAT32: ret: 000054f3, offset: 00f2 FAT32: entry: 0x54f3 = 21747, offset: 0x00f3 = 243 FAT32: ret: 000054f4, offset: 00f3 FAT32: entry: 0x54f4 = 21748, offset: 0x00f4 = 244 FAT32: ret: 000054f5, offset: 00f4 FAT32: entry: 0x54f5 = 21749, offset: 0x00f5 = 245 FAT32: ret: 000054f6, offset: 00f5 FAT32: entry: 0x54f6 = 21750, offset: 0x00f6 = 246 FAT32: ret: 000054f7, offset: 00f6 FAT32: entry: 0x54f7 = 21751, offset: 0x00f7 = 247 FAT32: ret: 000054f8, offset: 00f7 FAT32: entry: 0x54f8 = 21752, offset: 0x00f8 = 248 FAT32: ret: 000054f9, offset: 00f8 FAT32: entry: 0x54f9 = 21753, offset: 0x00f9 = 249 FAT32: ret: 000054fa, offset: 00f9 FAT32: entry: 0x54fa = 21754, offset: 0x00fa = 250 FAT32: ret: 000054fb, offset: 00fa FAT32: entry: 0x54fb = 21755, offset: 0x00fb = 251 FAT32: ret: 000054fc, offset: 00fb FAT32: entry: 0x54fc = 21756, offset: 0x00fc = 252 FAT32: ret: 000054fd, offset: 00fc FAT32: entry: 0x54fd = 21757, offset: 0x00fd = 253 FAT32: ret: 000054fe, offset: 00fd FAT32: entry: 0x54fe = 21758, offset: 0x00fe = 254 FAT32: ret: 000054ff, offset: 00fe FAT32: entry: 0x54ff = 21759, offset: 0x00ff = 255 FAT32: ret: 00005500, offset: 00ff FAT32: entry: 0x5500 = 21760, offset: 0x0100 = 256 FAT32: ret: 00005501, offset: 0100 FAT32: entry: 0x5501 = 21761, offset: 0x0101 = 257 FAT32: ret: 00005502, offset: 0101 FAT32: entry: 0x5502 = 21762, offset: 0x0102 = 258 FAT32: ret: 00005503, offset: 0102 FAT32: entry: 0x5503 = 21763, offset: 0x0103 = 259 FAT32: ret: 00005504, offset: 0103 FAT32: entry: 0x5504 = 21764, offset: 0x0104 = 260 FAT32: ret: 00005505, offset: 0104 FAT32: entry: 0x5505 = 21765, offset: 0x0105 = 261 FAT32: ret: 00005506, offset: 0105 FAT32: entry: 0x5506 = 21766, offset: 0x0106 = 262 FAT32: ret: 00005507, offset: 0106 FAT32: entry: 0x5507 = 21767, offset: 0x0107 = 263 FAT32: ret: 00005508, offset: 0107 FAT32: entry: 0x5508 = 21768, offset: 0x0108 = 264 FAT32: ret: 00005509, offset: 0108 FAT32: entry: 0x5509 = 21769, offset: 0x0109 = 265 FAT32: ret: 0000550a, offset: 0109 FAT32: entry: 0x550a = 21770, offset: 0x010a = 266 FAT32: ret: 0000550b, offset: 010a FAT32: entry: 0x550b = 21771, offset: 0x010b = 267 FAT32: ret: 0000550c, offset: 010b FAT32: entry: 0x550c = 21772, offset: 0x010c = 268 FAT32: ret: 0000550d, offset: 010c FAT32: entry: 0x550d = 21773, offset: 0x010d = 269 FAT32: ret: 0000550e, offset: 010d FAT32: entry: 0x550e = 21774, offset: 0x010e = 270 FAT32: ret: 0000550f, offset: 010e FAT32: entry: 0x550f = 21775, offset: 0x010f = 271 FAT32: ret: 00005510, offset: 010f FAT32: entry: 0x5510 = 21776, offset: 0x0110 = 272 FAT32: ret: 00005511, offset: 0110 FAT32: entry: 0x5511 = 21777, offset: 0x0111 = 273 FAT32: ret: 00005512, offset: 0111 FAT32: entry: 0x5512 = 21778, offset: 0x0112 = 274 FAT32: ret: 00005513, offset: 0112 FAT32: entry: 0x5513 = 21779, offset: 0x0113 = 275 FAT32: ret: 00005514, offset: 0113 FAT32: entry: 0x5514 = 21780, offset: 0x0114 = 276 FAT32: ret: 00005515, offset: 0114 FAT32: entry: 0x5515 = 21781, offset: 0x0115 = 277 FAT32: ret: 00005516, offset: 0115 FAT32: entry: 0x5516 = 21782, offset: 0x0116 = 278 FAT32: ret: 00005517, offset: 0116 FAT32: entry: 0x5517 = 21783, offset: 0x0117 = 279 FAT32: ret: 00005518, offset: 0117 FAT32: entry: 0x5518 = 21784, offset: 0x0118 = 280 FAT32: ret: 00005519, offset: 0118 FAT32: entry: 0x5519 = 21785, offset: 0x0119 = 281 FAT32: ret: 0000551a, offset: 0119 FAT32: entry: 0x551a = 21786, offset: 0x011a = 282 FAT32: ret: 0000551b, offset: 011a FAT32: entry: 0x551b = 21787, offset: 0x011b = 283 FAT32: ret: 0000551c, offset: 011b FAT32: entry: 0x551c = 21788, offset: 0x011c = 284 FAT32: ret: 0000551d, offset: 011c FAT32: entry: 0x551d = 21789, offset: 0x011d = 285 FAT32: ret: 0000551e, offset: 011d FAT32: entry: 0x551e = 21790, offset: 0x011e = 286 FAT32: ret: 0000551f, offset: 011e FAT32: entry: 0x551f = 21791, offset: 0x011f = 287 FAT32: ret: 00005520, offset: 011f FAT32: entry: 0x5520 = 21792, offset: 0x0120 = 288 FAT32: ret: 00005521, offset: 0120 FAT32: entry: 0x5521 = 21793, offset: 0x0121 = 289 FAT32: ret: 00005522, offset: 0121 FAT32: entry: 0x5522 = 21794, offset: 0x0122 = 290 FAT32: ret: 00005523, offset: 0122 FAT32: entry: 0x5523 = 21795, offset: 0x0123 = 291 FAT32: ret: 00005524, offset: 0123 FAT32: entry: 0x5524 = 21796, offset: 0x0124 = 292 FAT32: ret: 00005525, offset: 0124 FAT32: entry: 0x5525 = 21797, offset: 0x0125 = 293 FAT32: ret: 00005526, offset: 0125 FAT32: entry: 0x5526 = 21798, offset: 0x0126 = 294 FAT32: ret: 00005527, offset: 0126 FAT32: entry: 0x5527 = 21799, offset: 0x0127 = 295 FAT32: ret: 00005528, offset: 0127 FAT32: entry: 0x5528 = 21800, offset: 0x0128 = 296 FAT32: ret: 00005529, offset: 0128 FAT32: entry: 0x5529 = 21801, offset: 0x0129 = 297 FAT32: ret: 0000552a, offset: 0129 FAT32: entry: 0x552a = 21802, offset: 0x012a = 298 FAT32: ret: 0000552b, offset: 012a FAT32: entry: 0x552b = 21803, offset: 0x012b = 299 FAT32: ret: 0000552c, offset: 012b FAT32: entry: 0x552c = 21804, offset: 0x012c = 300 FAT32: ret: 0000552d, offset: 012c FAT32: entry: 0x552d = 21805, offset: 0x012d = 301 FAT32: ret: 0000552e, offset: 012d FAT32: entry: 0x552e = 21806, offset: 0x012e = 302 FAT32: ret: 0000552f, offset: 012e FAT32: entry: 0x552f = 21807, offset: 0x012f = 303 FAT32: ret: 00005530, offset: 012f FAT32: entry: 0x5530 = 21808, offset: 0x0130 = 304 FAT32: ret: 00005531, offset: 0130 FAT32: entry: 0x5531 = 21809, offset: 0x0131 = 305 FAT32: ret: 00005532, offset: 0131 FAT32: entry: 0x5532 = 21810, offset: 0x0132 = 306 FAT32: ret: 00005533, offset: 0132 FAT32: entry: 0x5533 = 21811, offset: 0x0133 = 307 FAT32: ret: 00005534, offset: 0133 FAT32: entry: 0x5534 = 21812, offset: 0x0134 = 308 FAT32: ret: 00005535, offset: 0134 FAT32: entry: 0x5535 = 21813, offset: 0x0135 = 309 FAT32: ret: 00005536, offset: 0135 FAT32: entry: 0x5536 = 21814, offset: 0x0136 = 310 FAT32: ret: 00005537, offset: 0136 FAT32: entry: 0x5537 = 21815, offset: 0x0137 = 311 FAT32: ret: 00005538, offset: 0137 FAT32: entry: 0x5538 = 21816, offset: 0x0138 = 312 FAT32: ret: 00005539, offset: 0138 FAT32: entry: 0x5539 = 21817, offset: 0x0139 = 313 FAT32: ret: 0000553a, offset: 0139 FAT32: entry: 0x553a = 21818, offset: 0x013a = 314 FAT32: ret: 0000553b, offset: 013a FAT32: entry: 0x553b = 21819, offset: 0x013b = 315 FAT32: ret: 0000553c, offset: 013b FAT32: entry: 0x553c = 21820, offset: 0x013c = 316 FAT32: ret: 0000553d, offset: 013c FAT32: entry: 0x553d = 21821, offset: 0x013d = 317 FAT32: ret: 0000553e, offset: 013d FAT32: entry: 0x553e = 21822, offset: 0x013e = 318 FAT32: ret: 0000553f, offset: 013e FAT32: entry: 0x553f = 21823, offset: 0x013f = 319 FAT32: ret: 00005540, offset: 013f FAT32: entry: 0x5540 = 21824, offset: 0x0140 = 320 FAT32: ret: 00005541, offset: 0140 FAT32: entry: 0x5541 = 21825, offset: 0x0141 = 321 FAT32: ret: 00005542, offset: 0141 FAT32: entry: 0x5542 = 21826, offset: 0x0142 = 322 FAT32: ret: 00005543, offset: 0142 FAT32: entry: 0x5543 = 21827, offset: 0x0143 = 323 FAT32: ret: 00005544, offset: 0143 FAT32: entry: 0x5544 = 21828, offset: 0x0144 = 324 FAT32: ret: 00005545, offset: 0144 FAT32: entry: 0x5545 = 21829, offset: 0x0145 = 325 FAT32: ret: 00005546, offset: 0145 FAT32: entry: 0x5546 = 21830, offset: 0x0146 = 326 FAT32: ret: 00005547, offset: 0146 FAT32: entry: 0x5547 = 21831, offset: 0x0147 = 327 FAT32: ret: 00005548, offset: 0147 FAT32: entry: 0x5548 = 21832, offset: 0x0148 = 328 FAT32: ret: 00005549, offset: 0148 FAT32: entry: 0x5549 = 21833, offset: 0x0149 = 329 FAT32: ret: 0000554a, offset: 0149 FAT32: entry: 0x554a = 21834, offset: 0x014a = 330 FAT32: ret: 0000554b, offset: 014a FAT32: entry: 0x554b = 21835, offset: 0x014b = 331 FAT32: ret: 0000554c, offset: 014b FAT32: entry: 0x554c = 21836, offset: 0x014c = 332 FAT32: ret: 0000554d, offset: 014c FAT32: entry: 0x554d = 21837, offset: 0x014d = 333 FAT32: ret: 0000554e, offset: 014d FAT32: entry: 0x554e = 21838, offset: 0x014e = 334 FAT32: ret: 0000554f, offset: 014e FAT32: entry: 0x554f = 21839, offset: 0x014f = 335 FAT32: ret: 00005550, offset: 014f FAT32: entry: 0x5550 = 21840, offset: 0x0150 = 336 FAT32: ret: 00005551, offset: 0150 FAT32: entry: 0x5551 = 21841, offset: 0x0151 = 337 FAT32: ret: 00005552, offset: 0151 FAT32: entry: 0x5552 = 21842, offset: 0x0152 = 338 FAT32: ret: 00005553, offset: 0152 FAT32: entry: 0x5553 = 21843, offset: 0x0153 = 339 FAT32: ret: 00005554, offset: 0153 FAT32: entry: 0x5554 = 21844, offset: 0x0154 = 340 FAT32: ret: 00005555, offset: 0154 FAT32: entry: 0x5555 = 21845, offset: 0x0155 = 341 FAT32: ret: 00005556, offset: 0155 FAT32: entry: 0x5556 = 21846, offset: 0x0156 = 342 FAT32: ret: 00005557, offset: 0156 FAT32: entry: 0x5557 = 21847, offset: 0x0157 = 343 FAT32: ret: 00005558, offset: 0157 FAT32: entry: 0x5558 = 21848, offset: 0x0158 = 344 FAT32: ret: 00005559, offset: 0158 FAT32: entry: 0x5559 = 21849, offset: 0x0159 = 345 FAT32: ret: 0000555a, offset: 0159 FAT32: entry: 0x555a = 21850, offset: 0x015a = 346 FAT32: ret: 0000555b, offset: 015a FAT32: entry: 0x555b = 21851, offset: 0x015b = 347 FAT32: ret: 0000555c, offset: 015b FAT32: entry: 0x555c = 21852, offset: 0x015c = 348 FAT32: ret: 0000555d, offset: 015c FAT32: entry: 0x555d = 21853, offset: 0x015d = 349 FAT32: ret: 0000555e, offset: 015d FAT32: entry: 0x555e = 21854, offset: 0x015e = 350 FAT32: ret: 0000555f, offset: 015e FAT32: entry: 0x555f = 21855, offset: 0x015f = 351 FAT32: ret: 00005560, offset: 015f FAT32: entry: 0x5560 = 21856, offset: 0x0160 = 352 FAT32: ret: 00005561, offset: 0160 FAT32: entry: 0x5561 = 21857, offset: 0x0161 = 353 FAT32: ret: 00005562, offset: 0161 FAT32: entry: 0x5562 = 21858, offset: 0x0162 = 354 FAT32: ret: 00005563, offset: 0162 FAT32: entry: 0x5563 = 21859, offset: 0x0163 = 355 FAT32: ret: 00005564, offset: 0163 FAT32: entry: 0x5564 = 21860, offset: 0x0164 = 356 FAT32: ret: 00005565, offset: 0164 FAT32: entry: 0x5565 = 21861, offset: 0x0165 = 357 FAT32: ret: 00005566, offset: 0165 FAT32: entry: 0x5566 = 21862, offset: 0x0166 = 358 FAT32: ret: 00005567, offset: 0166 FAT32: entry: 0x5567 = 21863, offset: 0x0167 = 359 FAT32: ret: 00005568, offset: 0167 FAT32: entry: 0x5568 = 21864, offset: 0x0168 = 360 FAT32: ret: 00005569, offset: 0168 FAT32: entry: 0x5569 = 21865, offset: 0x0169 = 361 FAT32: ret: 0000556a, offset: 0169 FAT32: entry: 0x556a = 21866, offset: 0x016a = 362 FAT32: ret: 0000556b, offset: 016a FAT32: entry: 0x556b = 21867, offset: 0x016b = 363 FAT32: ret: 0000556c, offset: 016b FAT32: entry: 0x556c = 21868, offset: 0x016c = 364 FAT32: ret: 0000556d, offset: 016c FAT32: entry: 0x556d = 21869, offset: 0x016d = 365 FAT32: ret: 0000556e, offset: 016d FAT32: entry: 0x556e = 21870, offset: 0x016e = 366 FAT32: ret: 0000556f, offset: 016e FAT32: entry: 0x556f = 21871, offset: 0x016f = 367 FAT32: ret: 00005570, offset: 016f FAT32: entry: 0x5570 = 21872, offset: 0x0170 = 368 FAT32: ret: 00005571, offset: 0170 FAT32: entry: 0x5571 = 21873, offset: 0x0171 = 369 FAT32: ret: 00005572, offset: 0171 FAT32: entry: 0x5572 = 21874, offset: 0x0172 = 370 FAT32: ret: 00005573, offset: 0172 FAT32: entry: 0x5573 = 21875, offset: 0x0173 = 371 FAT32: ret: 00005574, offset: 0173 FAT32: entry: 0x5574 = 21876, offset: 0x0174 = 372 FAT32: ret: 00005575, offset: 0174 FAT32: entry: 0x5575 = 21877, offset: 0x0175 = 373 FAT32: ret: 00005576, offset: 0175 FAT32: entry: 0x5576 = 21878, offset: 0x0176 = 374 FAT32: ret: 00005577, offset: 0176 FAT32: entry: 0x5577 = 21879, offset: 0x0177 = 375 FAT32: ret: 00005578, offset: 0177 FAT32: entry: 0x5578 = 21880, offset: 0x0178 = 376 FAT32: ret: 00005579, offset: 0178 FAT32: entry: 0x5579 = 21881, offset: 0x0179 = 377 FAT32: ret: 0000557a, offset: 0179 FAT32: entry: 0x557a = 21882, offset: 0x017a = 378 FAT32: ret: 0000557b, offset: 017a FAT32: entry: 0x557b = 21883, offset: 0x017b = 379 FAT32: ret: 0000557c, offset: 017b FAT32: entry: 0x557c = 21884, offset: 0x017c = 380 FAT32: ret: 0000557d, offset: 017c FAT32: entry: 0x557d = 21885, offset: 0x017d = 381 FAT32: ret: 0000557e, offset: 017d FAT32: entry: 0x557e = 21886, offset: 0x017e = 382 FAT32: ret: 0000557f, offset: 017e FAT32: entry: 0x557f = 21887, offset: 0x017f = 383 FAT32: ret: 00005580, offset: 017f FAT32: entry: 0x5580 = 21888, offset: 0x0180 = 384 FAT32: ret: 00005581, offset: 0180 FAT32: entry: 0x5581 = 21889, offset: 0x0181 = 385 FAT32: ret: 00005582, offset: 0181 FAT32: entry: 0x5582 = 21890, offset: 0x0182 = 386 FAT32: ret: 00005583, offset: 0182 FAT32: entry: 0x5583 = 21891, offset: 0x0183 = 387 FAT32: ret: 00005584, offset: 0183 FAT32: entry: 0x5584 = 21892, offset: 0x0184 = 388 FAT32: ret: 00005585, offset: 0184 FAT32: entry: 0x5585 = 21893, offset: 0x0185 = 389 FAT32: ret: 00005586, offset: 0185 FAT32: entry: 0x5586 = 21894, offset: 0x0186 = 390 FAT32: ret: 00005587, offset: 0186 FAT32: entry: 0x5587 = 21895, offset: 0x0187 = 391 FAT32: ret: 00005588, offset: 0187 FAT32: entry: 0x5588 = 21896, offset: 0x0188 = 392 FAT32: ret: 00005589, offset: 0188 FAT32: entry: 0x5589 = 21897, offset: 0x0189 = 393 FAT32: ret: 0000558a, offset: 0189 FAT32: entry: 0x558a = 21898, offset: 0x018a = 394 FAT32: ret: 0000558b, offset: 018a FAT32: entry: 0x558b = 21899, offset: 0x018b = 395 FAT32: ret: 0000558c, offset: 018b FAT32: entry: 0x558c = 21900, offset: 0x018c = 396 FAT32: ret: 0000558d, offset: 018c FAT32: entry: 0x558d = 21901, offset: 0x018d = 397 FAT32: ret: 0000558e, offset: 018d FAT32: entry: 0x558e = 21902, offset: 0x018e = 398 FAT32: ret: 0000558f, offset: 018e FAT32: entry: 0x558f = 21903, offset: 0x018f = 399 FAT32: ret: 00005590, offset: 018f FAT32: entry: 0x5590 = 21904, offset: 0x0190 = 400 FAT32: ret: 00005591, offset: 0190 FAT32: entry: 0x5591 = 21905, offset: 0x0191 = 401 FAT32: ret: 00005592, offset: 0191 FAT32: entry: 0x5592 = 21906, offset: 0x0192 = 402 FAT32: ret: 00005593, offset: 0192 FAT32: entry: 0x5593 = 21907, offset: 0x0193 = 403 FAT32: ret: 00005594, offset: 0193 FAT32: entry: 0x5594 = 21908, offset: 0x0194 = 404 FAT32: ret: 00005595, offset: 0194 FAT32: entry: 0x5595 = 21909, offset: 0x0195 = 405 FAT32: ret: 00005596, offset: 0195 FAT32: entry: 0x5596 = 21910, offset: 0x0196 = 406 FAT32: ret: 00005597, offset: 0196 FAT32: entry: 0x5597 = 21911, offset: 0x0197 = 407 FAT32: ret: 00005598, offset: 0197 FAT32: entry: 0x5598 = 21912, offset: 0x0198 = 408 FAT32: ret: 00005599, offset: 0198 FAT32: entry: 0x5599 = 21913, offset: 0x0199 = 409 FAT32: ret: 0000559a, offset: 0199 FAT32: entry: 0x559a = 21914, offset: 0x019a = 410 FAT32: ret: 0000559b, offset: 019a FAT32: entry: 0x559b = 21915, offset: 0x019b = 411 FAT32: ret: 0000559c, offset: 019b FAT32: entry: 0x559c = 21916, offset: 0x019c = 412 FAT32: ret: 0000559d, offset: 019c FAT32: entry: 0x559d = 21917, offset: 0x019d = 413 FAT32: ret: 0000559e, offset: 019d FAT32: entry: 0x559e = 21918, offset: 0x019e = 414 FAT32: ret: 0000559f, offset: 019e FAT32: entry: 0x559f = 21919, offset: 0x019f = 415 FAT32: ret: 000055a0, offset: 019f FAT32: entry: 0x55a0 = 21920, offset: 0x01a0 = 416 FAT32: ret: 000055a1, offset: 01a0 FAT32: entry: 0x55a1 = 21921, offset: 0x01a1 = 417 FAT32: ret: 000055a2, offset: 01a1 FAT32: entry: 0x55a2 = 21922, offset: 0x01a2 = 418 FAT32: ret: 000055a3, offset: 01a2 gc - clustnum: 21392, startsect: 23646 Size: 271996, got: 271996 Jumping to U-Boot image entry point: 0x80800000