Hi all:
I develop on dm8168 with dvrrdk3.50.And I want to boot from eth1,and download uImage from
eth1,and run nfs system on eth1 port, all of which are done on eth0,
How can i do this? the uboot ,kernel must be updated ?
best regards
xavier
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all:
I develop on dm8168 with dvrrdk3.50.And I want to boot from eth1,and download uImage from
eth1,and run nfs system on eth1 port, all of which are done on eth0,
How can i do this? the uboot ,kernel must be updated ?
best regards
xavier
Hi,
Is this your custom board or TI's EVM ?
How can i do this? the uboot ,kernel must be updated ?
Yes, By default the either MII or RMII ethernet could configured in EVM board and need to change in u-boot (def file) as well as linux (board file) if you want access other eth port,
Need to disable eth1 and then enable eth0,,