This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OSC0 Crystal the max Start-up time on AM3352

Guru 16800 points

Other Parts Discussed in Thread: AM3352

Hello,

Could you teach me the max Start-up time for OSC0 Crystal on AM3352?
At Table 4-3 in datasheet, tsx (Start-up time) is described the only TYP value.

Best Regards.

Nomoto

  • Oscillator start-up time depends on many product specific variables like the crystal circuit components, PCB layout, and operating conditions.  Therefore, it is not possible to provide a maximum value for this parameter.

    System level characterization of the product across all operating conditions would need to be performed to determine the maximum oscillator start-up time.

    Regards,
    Paul