Looking at the DM8168 datasheet, page 139 shows the "Electrical Characteristics" table. It lists a minimum Voh (for 3.3V I/O) of 2.4V at the maximum output current (6mA). I am not operating anywhere near that - I'm more like 100uA instead.
My problem is that one of the devices the DM8168 is talking to has a minimum Vih of Vcc-0.3V (or 3.0V in my case). Therefore, I can't guarantee operation when using 2.4V Voh for the DM8168.
My main question is, what is the DM8168's minimum Voh (for 3.3V I/O) for a 100uA output current?
Thanks!
-Bill