I am working on a project that there is a 7" touch LCD on it. I want to driver this LCD with a module which has an operating system on it. Because device's mission is very simple. Just showing a video on LCD and when a user touch this LCD, the device opens a few outputs. The quantity is not too much so i want to solve this problem by using development kits' module, daughter boards..etc. I will design a mother board. The mosfets and relays will be on this board. I want to put the module on this board. This module will have an operating system and can drive a 7" LCD. Maybe I want too much :) but this is the best way i guess. Can you suggest and board, module, daughter module ...etc to me?
Or if you have any idea to solve this problem please tell me?