Dear Sir/Madam,
We are using the TMS320DM814x processor in our project.
We have used the linux kernel with PSP patch: linux-2.6.37-psp04.04.00.01
Further,we have compiled the kernel with following options
1."[*]Device Drivers"->"Network device support"->"PHY Device support and infrastructure"- - - >"Drivers for Marvell PHYs" ( Marvell - We used the custom PHY driver).
2.[*] Networking support ---> Device Drivers --->
[*]Network device support --->[*] Ethernet driver support --->
-*- TI DaVinci MDIO Support
-*- TI DaVinci CPDMA Support
-*- TI CPSW Switch Phy sel Support
<*> TI CPSW Switch Support
For the above configuration of kernel and booted with that image,After assigned the Ip address for the eth0 and try to ping.
The ping not working.When we seen the dmesg in the kernel log it shows the following log
Starting Bootlog daemon: bootlogd.
Configuring network interfaces... PHY 0:00 not found
CPSW phy found : id is : 0x1410dd1
udhcpc (v1.19.4) started
Sending discover...
PHY: 0:01 - Link is Up - 100/Full
Sending discover...
Sending discover...
No lease, failing
done.
Another observation is,when we tried to connect the board with PC both are locally connected by point to point.
When we tried the PING between these nodes We couldnt receive any packet capture observed in wireshark.
Could you help us to resolve this issue.
thanks
senthil nathan..