This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CMOS Sensors connections to VIP0 and VIP1



Dear Support,

We are designing a board with the DM8148 and we will be using at the same time Two sensors:

Aptina MT9 M031 12 bit with external sync signals

Aptina MT9 MP31 12 bit with external sync signals

Is there any application or document that shows how to connect this type of sensors using both of the video input ports?

This is the last issue we have on this design.

sandro