Other Parts Discussed in Thread: DP83848M, AM3354
Our board using am3354 + DP83848M (in MII mode). There is problem in the PHY. There is loopback mode provided on DP83848M to loop back the MMI data interface. But, how can I do the test on am3354 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eric,
As you can see from running "ifconfig -a", the Local Loopback is the "lo" interface with inet address 127.0.0.1. Ping it:
ping localhost
Best regards,
Miroslav
Hi Miroslav,
I found out that even if I remove the LAN cable from the RJ45 and I didn't turn on any loopback on the PHY transceiver, ping 127.0.0.1 still works. Moreover, our system has both WiFi and ethernet interfaces. But, 127.0.0.1 is a single loopback interface. Hence, I think the 127.0.0.1 loopback interface should be in a higher level inside the Linux. No packet will be sent out to either WiFi controller nor the PHY transceiver. Is my understanding correct ?
Eric, I'm sorry I didn't understand you the first time. Try using the "ethtool" command to test your interface:
ethtool -t DEVNAME
Best regards,
Miroslav
Hi Miroslav,
Thanks to your advice ! That's really great. But, unfortunately, the ethtool coming along with the Linux for my am3354 doesn't support ethtool -t. It replied "Operation not supported". Do you know where I can get the version ethtool (no matter executable binary or ipk) that allows me to run 'ethtool -t' ?
Eric, I'm sorry, but it seems like the cpsw driver doesn't support ethtool testing:
root@am335x-evm:~# ethtool -i eth0
driver: TI CPSW Driver v1.0
version: 1.0
firmware-version:
bus-info: cpsw
supports-statistics: no
supports-test: no
supports-eeprom-access: no
supports-register-dump: no
supports-priv-flags: no
Best regards,
Miroslav
Miroslav,
Is there any way to override this setting in cpsw ? Can I re-enable it by modifying the source codes / compiler switch and then re-compile the kernel ? This is important to me, because our project gets stuck on the PHY. We have to overcome it.
Thanks !
Eric, I'll try to escalate this to the factory team and see if they can suggest something.
Best regards,
Miroslav
Miroslav,
Is there any update on how to enable testing in cpsw ?
Looking forward to your reply.
Thanks !
Eric