Other Parts Discussed in Thread: TMS320DM6437
Hi,
Is there any example codes like stellarisware,starterware for TMS320DM6437 ?.
I found and installed C6748_StarterWare_1_20_04_01 , but it is shows lot of linker errors when i changed the processor from C6748 to DM6437.
Is C6748_StarterWare_1_20_04_01 is the correct Example codes for TMS320DM6437 ? If so can anyone help me to port this to TMS320DM6437 .
Actually i want to use UART,GPIO,NAND etc example codes for my project.
Thanks and regards,
Shihab