Other Parts Discussed in Thread: AM3352
Hi,
We are planning to interface Micron’s MT41K256M16HA-125 IT:E DDR3 with Texas Instruments AM3352 processor. There will be only one DDR3 device on our board so we are not planning to provide VTT (flyby) termination as it will be a point to point topology. All the address and control signals will be routed as per the DDR3 routing guidelines given in AM3352 datasheet. The frequency of operation will be 400MHz DDR3 Clock. Also the ambient operating temperature for the board is -40C to 85C.
- Can you please confirm if DDR3 design without VTT will provide acceptable signal integrity if the DDR device is kept near to processor and routing guidelines followed as mentioned in datasheet?
- Do you foresee any signal integrity issues at the extreme temperatures without VTT termination on board?
Thanks & regards,
Nikhil