This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Booting problem with omap5



Hi,

I am trying to run Linux on the board using an sd card.

When I boot the board I get the following ( and no more output after 'Starting kernel').

U-Boot SPL 2013.01-gdc6238c (Mar 27 2013 - 14:33:47)
OMAP5432 ES2.0
die_id1: 15d6074
lisa_map_2: 0x80740300
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img


U-Boot 2013.01-gdc6238c (Mar 27 2013 - 14:33:47)

CPU  : OMAP5432 ES2.0
Board: OMAP5430 EVM
I2C:   ready
DRAM:  2 GiB
relocation Offset is: 7e101000
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
In:    serial
Out:   serial
Err:   serial
Hit any key to stop autoboot:  0
reading omap5-uevm.dtb
42953 bytes read in 11 ms (3.7 MiB/s)
reading uImage
4466736 bytes read in 287 ms (14.8 MiB/s)
## Booting kernel from Legacy Image at 80300000 ...
   Image Name:   Linux-3.13.0-rc7-g692ddae
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    4466672 Bytes = 4.3 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 825f0000
   Booting using the fdt blob at 0x825f0000
   Loading Kernel Image ... OK
OK
   Loading Device Tree to feef2000, end feeff7c8 ... OK

Starting kernel ...

If anyone knows what's the problem.

Thanks

  • Hello,

    Which GLSDK are you using?

    There is a limitation of OMAP5 GLSDKs, that says: OMAPS00305059: Omap5 is not getting booted if the ethernet cable is not connected (see http://processors.wiki.ti.com/index.php/OMAP5_GLSDK_6.03.00.01_Release_Notes)

    Have you followed the GLSDK software developers guide (http://processors.wiki.ti.com/index.php/OMAP5_GLSDK_Software_Developers_Guide), when building your MLO, u-boot & kernel?

    Best Regards,

    Yordan

  • Hello Yordan,

    I am using the GLSDK 6.00.00.07. I connected the ethernet cable but it didn't fix the problem.

    I followed the virtual open systems guide http://www.virtualopensystems.com/en/solutions/guides/kvm-svirt-omap5/.

    I used precompiled kernel image and dtb file.

    Thanks.

  • Hi,

    A couple of suggestions bellow:

    1. This could be a problem with the power supply of the board; it should be DC12V as suggested in the quick start guide: http://downloads.ti.com/dsps/dsps_public_sw/glsdk/6_01_00_01/exports/OMAP5_ES_2_0_Quick_Start_Guide.pdf 

    I personally work with DC5V 2.0A power supply on my board.

    2. I am not familiar with the virtual open system guide... Please make sure you follow the instructions in GLSDK software developers guide: http://processors.wiki.ti.com/index.php/OMAP5_GLSDK_Software_Developers_Guide#Starting_your_software_development

    And use the prebuilt images from the board-support/prebuilt-images/ folder.

    3. Just for a test you can try some of the later versions of GLSDK: http://downloads.ti.com/dsps/dsps_public_sw/glsdk/6_01_00_01/index_FDS.html , although I've tested GLSDK6_00 on my board so it should work.

    Best Regards,

    Yordan