Hi TI team
please I have two questions .. i would be grateful if you answer them
1) when i begin debuging the tcp3e example this sentence appears up and repeated 16 times
[C66xx_0] WORKAROUND: Forced queue push address from (0x3402000c) to (0x2a2000c)
and stop showing any action on console window ... beside that in debug window the c6670 still running
and didn't show any error in console window ... so what is it mean ?? and how can i handle this ??
2) If we agree that the cfg , the info and the coded bits are in the test example folder in the form of files and the example code call them and compare with the coded bits ... so how can i change the cfg and info bits in the absence of declaration of the parameters in these files and off course by changing the info and cfg bits the coded bits will change so how the example TCP3E will handle with this ...
thx alot