Other Parts Discussed in Thread: TMS320C6655, TMDSEVM6657, TMS320C6657
We are currently evaluating the TMS320C6655 device for our next product . We started some preliminary bring-up and evaluation of DSP EVM over past couple of months and are now wanting to interconnect a Xilinx SP605 evaluation board to one of your TMDSEVM6657 Lite Evaluation Modules. We have decided that the high speed interface that we believe makes the most since to stream data and keep overhead/cost down on FPGA side is PCIe but open to other suggestions. Note: I have not used PCIe before in a design. The TMDSEVM6657 support 1 or 2 lanes of PCIe over AMC edge card connector. The eInfoChip AMC to PCIe Adapter Brd appears to support 4 lanes? Basically we want to tap into a single PCIe lane on TMDSEVM6657 and connect to Xilinx SP605 which supports x1 PCIe lane edge connector. The Xilinx FPGA (SP605 Eval Brd in this scenario) in actual system would be processing and streaming packetized data to single lane of TMDSEVM6657. We need a way for prototype system using EVMs to interconnect Xilinx SP605 x1 PCIe lane to single lane of PCIe on AMC edge card connector of TMDSEVM6657. I am trying to determine the best way to get there and if eInfoChip AMC to PCIe adapter card simplifies solution or if we should develop a data card. Any suggestions would be greatly appreciated.