I'm testing my ddr3 module but i see a strange behaviour, a sort of Wrap Around of the memory.
Im testing the first 2 GB of my 8GB Kingston DDR3 Memory
Starting from the beginning of the Address (8x00000000) i'm able to write and read correctly up to 1GB of pseudo-random data without errors.
But if i try to write and read 2GB of data i see that the second GB is exactly the same of the first, as if after the address 8x40000000 the DSP start again writing from 8x00000000.
I still haven't changed the default setting for the MPAX for the DDR3 data memory space so i should be able to access to all the first 2 GB of the DDR3.
What could be the problem?
Thanks