This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error in DM6446 project (when use opencv)



hi everyone

My project involves a detection algorithm , and I have developed this algorithm by using
opencv. Now,I want to use DM6446 device and its software to implement my project .

My project is based on video_copy example which contains three folders :codec, server,
video_copy_app,and I have done some changes as below:

The first step: I have establish a project in ccs3.3 to generated a static lib , then
download emcv (opencv embedded version ) , after complied,it generates
cv.lib and cxcore.lib.

Step Two: In the 'codec' folder, I open the file 'videnc_copy.c ',then insert my algorithm
code, which uses 5 opencv function .
when Compiled codec, their is no error.

The third step : In the 'server' folder,I open the file 'link.cmd', then add the statement
"-l cv.lib cxcore.lib"

When compiled,there is no error but appear a lot warning. as below:
>> Warning: function definitions in CSU declarations are not supported
>> Warning: missing DW_AT_name attribute

Step 4: In the 'videocopy.app' floder,I open the file ' video.c' , and set up a counter
whose function is conut to 20 , and then transferred a frame of video to process.

when running the program, it stoped and the console did not respond . Debug information is
as follows

Encodedecode Debug: 3 capture buffers were successfully allocated.
Encodedecode Debug: Capture driver buffer 0 at physical address 1138569216 mapp0
Encodedecode Debug: Capture driver buffer 1 at physical address 1139453952 mapp0
Encodedecode Debug: Capture driver buffer 2 at physical address 1140338688 mapp0
Encodedecode Debug: Video capture initialized and started
Smooth Debug: Creating smooth job of size 512x512
Encodedecode Debug: User interface created
Encodedecode Debug: Entering capture main loop.
Encodedecode Debug: Entering control main loop.
Encodedecode Debug: Entering display main loop.

I do not know where is the problem. compile error of cv.lib, cxcore.lib? or my
video_copy project settings wrong?

as to cv.lib and cxcore.lib, I created a project in ccs3.3 about dm6446 , it included the
main.c which contains my opencv algorithm.And the project is connected to the two
libraries . After complied、build、run ,it produced a correct result. (but the same code
when inserted to the file 'videnc_copy.c, woule die.)

I have tried to modify 'tcf' file in server folder, tried to modify CMEM allocated memory
pool ,but it does't work.

and I have the following questions :
1 To modify the tcf file,which guide can help me to fetch information .
2. How to use GT_Trace to debug the codes in dsp side.
3. how to get and use TI own image library of algorithms

I appreciate your information、advice! thank you so much!
(sorry for my poor english)

information of my board and software
my board based on DM6446, DRAM 128M, nand flash 128M.
bios_5_31_01 cg6x_6_0_14 cmem_1_02 codec_engine_1_10_01
codec_server_1_23 dsplink_1_30_08_02 xdais_5_10 xdc_2_94