Hello Sir
I hope to raise network ethernet bandwidth performence.
I tested network bandwidth, using iperf program.
device Information :
- cpu : am3359evm
- ethernet support 10/100/1000Mbps
- board is using brctl bridge util (ex. eth0-br0-eth1), use iptables.library.
test process :
#output format : 1000 Mbps
1. PC-PC test : bandwidth is about 640~720 Mbps
2. PC-BOARD-PC : bandwidth is about240~300 Mbps
3. PC-BOARD : bandwidth is about 264 Mbps
Can I upgrade network bandwidth performence? (e.g configure kernel, or iptables setting, etc)
When transfering large packet, I wish prevent packet loss.
it's my goal.