Hi all,
I want to receive large JPEG stream(1MByte) through the parallel Interface.
(as described in the TRM, Camera Interface Subsystem(ISP) 1.2.4.2 Parallel Generic Configuration: JPEG Sensor Connection on the Parallel Interface)
By setting the ISP_CTRL.JPEG_FLUSH bit, I can receive the JPEG stream less than 32kByte.
But the stream beyond 32kB is discarded.
$ hexdump jpegstream
0000000 d8ff e1ff d402 7845 6669 0000 4d4d 2a00
0000010 0000 0800 0900 0f01 0200 0000 1000 0000
0000020 7a00 1001 0200 0000 1000 0000 8a00 1201
...
0007fe0 7d30 5785 c50d 933a 58b8 036b 298e 7615
0007ff0 4c9a 8c10 ada3 bb30 c503 503f 7c6c 9164
0008000 0000 0000 0000 0000 0000 0000 0000 0000
...
I guess that it depends on CCDC_HORZ_INFO.NPH field. ( my setting is 0x7FFF currently )
How can I receive JPEG stream more than 32kB?