Other Parts Discussed in Thread: AM3352
Hi ,
I am using AM3352 processor & connecting it to NOR flash of Multiplexed address data 16bit
Also following the TRM-GPMC Table 7.5 @ page 269 & 270 , i have to map NOR DEVICE A(16-26) with GPMC A(1-10) & A27
But the Pin mux utility tool showing IO SET violation on using GPMC A(1-10)_mux0 ; so i have used GPMC A(1-10)_MUX1
Please confirm why am getting IO SET VIOLATION on using MUX0 pins of GPMC A(1-10) and also confirm whether it is ok to have gpmc a(1-10)_mux1 {the left put option} ?
Thanks & Regards
Jones