This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352 starter kit TPS65910 PWRHOLD

Other Parts Discussed in Thread: TPS65910, TPS65910A

Hi,

In the starter kit EVM the power hold pin of PMIC is connected to a pull up with VAUX33 supply. The user guide of TPS65910 (SWCU093C) has the timings in which the PWRHOLD should ramp when VRTC is stable. then other supplies ramp up. But when the board is powered on the VAUX33 supply will not be present and because of internal pull down the PWRHOLD will remain low.

In this case how the PMIC starts? is there any internal setting required for neglecting the PWRHOLD during the start up?

Thanks & Regards,

Nikhil