This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[SOLVED] Linux 3.12 on AM335x NAND flash device tree... need help !

Other Parts Discussed in Thread: AM3352

Hi All, 

I am trying to make a NAND flash working on a AM3352 custom board with the new 3.12 kernel. 

As discussed in a previous post, this custom board is tested and running on kernel 3.2, we can consider the hardware as validated.

I tried to configure the kernel with same features as the 3.2, I will not detail the kernel configuration now. 

Please find below the device tree configuration, it is copied from the EVM device tree and corresponds also to the configuration in our board file for the 3.2 kernel. 

What I see now is that there is no apparent issue in the dmesg. NAND flash is detected and identified:
[    1.067929] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xdc (Micron MT29F4G08ABADAWP)

But when I list the /dev/mtd* I only have /dev/mtd0, /dev/mtd0ro and /dev/mtd0block0. 

Do someone know why I can't access the both partitions? In which file are the nodes created from the device tree partitions?

Thanks in advance, best regards

Sylvain


And another question about the gpmc range configuration that "maps" the CS0 to a "Physical address of mapping". What is this physical address of mapping ? And could someone explain me how to understand this part of documentation (Documentation/devicetree/bindings/bus/ti-gpmc.txt)

- ranges: Must be set up to reflect the memory layout with four
integer values for each chip-select line in use:

<cs-number> 0 <physical address of mapping> <size>

Currently, calculated values derived from the contents
of the per-CS register GPMC_CONFIG7 (as set up by the
bootloader) are used for the physical address decoding.
As this will change in the future, filling correct
values here is a requirement.


Here is the part of device tree dedicated to the gpmc and nand flash:

&gpmc {
  status = "okay";
  pinctrl-names = "default";
  pinctrl-0 = <&nand_pins_default>;
  ranges = <0 0 0x08000000 0x20000000>; /* CS0: NAND 512MB size, mapping addr copied from EVM ??*/

  nand@0,0 {
    ti,elm-id = <&elm>;
    reg = <0 0 0>; /* CS0, offset 0 */
    nand-bus-width = <8>;
    ti,nand-ecc-opt = "bch8";
    gpmc,device-width = <1>;
    gpmc,sync-clk-ps = <0>;
    gpmc,cs-on-ns = <0>;
    gpmc,cs-rd-off-ns = <44>;
    gpmc,cs-wr-off-ns = <44>;
    gpmc,adv-on-ns = <6>;
    gpmc,adv-rd-off-ns = <34>;
    gpmc,adv-wr-off-ns = <44>;
    gpmc,we-on-ns = <0>;
    gpmc,we-off-ns = <40>;
    gpmc,oe-on-ns = <0>;
    gpmc,oe-off-ns = <54>;
    gpmc,access-ns = <64>;
    gpmc,rd-cycle-ns = <82>;
    gpmc,wr-cycle-ns = <82>;
    gpmc,wr-access-ns = <40>;
    gpmc,wr-data-mux-bus-ns = <0>;
    gpmc,wait-on-read = "true";
    gpmc,wait-on-write = "true";
    gpmc,bus-turnaround-ns = <0>;
    gpmc,cycle2cycle-delay-ns = <0>;
    gpmc,clk-activation-ns = <0>;
    gpmc,wait-monitoring-ns = <0>;

    #address-cells = <1>;
    #size-cells = <1>;

    /* partitions go here */
    partition@1 {
    label = "BOOT";
      reg = <0x00000000 0x04000000>;
    };

    partition@2 {
      label = "ROOTFS";
      reg = <0x04000000 0x1c000000>;
    };
  };
};

  • I found the solution...

    The "OpenFirmware partitioning information support" (CONFIG_MTD_OF_PARTS) was missing in my kernel... 

    I am getting tired of debugging the device tree... I think that debugging a feature that it's just not working is much harder with device tree, because we have to look very deep into the source files to understand how the DT is parsed and how functions are called, with which paramter... 

    To find this issue, I needed to look into drivers/mtd/ mtdcore.c, mtdpart.c and nand/omap2.c to understand that my device was added as a device and not as partitions. 

    I find the device tree solution very elegant, and powerfull for some applications. But it is time consuming and very complicated to understand how kernel is parsing the file...

    Next chapter... my PWM channel is not working... But it is configured in DT... I have to find why

  • Thanks for sharing your solution on the forum!